cancel
Showing results for 
Search instead for 
Did you mean: 

TIM13 and TIM14 PWM output issues STM32H562

dlewis
Associate II

Hi All,

I have a project that is using the STM32H562. I am having an issue using tim13 and tim14 to generate PWM outputs going to LEDs. The project uses timers tim2, tim3, tim4, tim13, and tim14 for a range of different PWM peripherals. For all of the timer instances that aren't tim13 and tim14, the PWM configures and works as expected, but I am unable to get any PWM output signal on the channels controlled by tim13 and tim14. Neither the autogenerated INIT functions or my application code to update the pulse width value return any errors from the HAL functions, and I can see the value of the registers being updated with the new pulse value, but there is no output on those pins. I have verified to some extent the hardware, because I am able to toggle those LED pins by configuring them as standard GPIO outputs and driving them high to see the LEDs illuminate. Any suggestions or information would be greatly appreciated! I can provide more information upon request. Thanks! 

16 REPLIES 16

Would suggest showing code, especially pin and TIM initialization code.

Ideally minimal/single function rather than CUBE spread it everywhere and obfuscated. Perhaps config TIM in lower frequency toggle mode rather than PWM

Enumerate the pins in use.

Perhaps inspect signals with a scope rather than LEDs / EYEs

Dump RCC, GPIO and TIM registers related to implementation

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hi, thanks for the reply! I'll add a couple more details and then get back to you with some simplified code to demonstrate the issue.

We did use a scope to check the output pins for PWM signal and it also demonstrated that the drivers were not behaving in the expected way as well. 
Here is the TIM3 auto generated INIT as an example of a PWM peripheral/timer that is working as expected

/* TIM3 init function */ void MX_TIM3_Init(void) { /* USER CODE BEGIN TIM3_Init 0 */ /* USER CODE END TIM3_Init 0 */ TIM_ClockConfigTypeDef sClockSourceConfig = {0}; TIM_MasterConfigTypeDef sMasterConfig = {0}; TIM_OC_InitTypeDef sConfigOC = {0}; /* USER CODE BEGIN TIM3_Init 1 */ /* USER CODE END TIM3_Init 1 */ htim3.Instance = TIM3; htim3.Init.Prescaler = 3; htim3.Init.CounterMode = TIM_COUNTERMODE_UP; htim3.Init.Period = 1000; htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; if (HAL_TIM_Base_Init(&htim3) != HAL_OK) { Error_Handler(); } sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL; if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK) { Error_Handler(); } if (HAL_TIM_PWM_Init(&htim3) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK) { Error_Handler(); } sConfigOC.OCMode = TIM_OCMODE_PWM1; sConfigOC.Pulse = 0; sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH; sConfigOC.OCFastMode = TIM_OCFAST_DISABLE; if (HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_1) != HAL_OK) { Error_Handler(); } if (HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_2) != HAL_OK) { Error_Handler(); } if (HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_3) != HAL_OK) { Error_Handler(); } if (HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_4) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM3_Init 2 */ /* USER CODE END TIM3_Init 2 */ HAL_TIM_MspPostInit(&htim3); }
View more

Below are the TIM13 and TIM14 generated INITs for the pwm instances that aren't working

/* TIM13 init function */ void MX_TIM13_Init(void) { /* USER CODE BEGIN TIM13_Init 0 */ /* USER CODE END TIM13_Init 0 */ TIM_OC_InitTypeDef sConfigOC = {0}; /* USER CODE BEGIN TIM13_Init 1 */ /* USER CODE END TIM13_Init 1 */ htim13.Instance = TIM13; htim13.Init.Prescaler = 3; htim13.Init.CounterMode = TIM_COUNTERMODE_UP; htim13.Init.Period = 1000; htim13.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim13.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; if (HAL_TIM_Base_Init(&htim13) != HAL_OK) { Error_Handler(); } if (HAL_TIM_PWM_Init(&htim13) != HAL_OK) { Error_Handler(); } sConfigOC.OCMode = TIM_OCMODE_PWM1; sConfigOC.Pulse = 0; sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH; sConfigOC.OCFastMode = TIM_OCFAST_DISABLE; if (HAL_TIM_PWM_ConfigChannel(&htim13, &sConfigOC, TIM_CHANNEL_1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM13_Init 2 */ /* USER CODE END TIM13_Init 2 */ HAL_TIM_MspPostInit(&htim13); } /* TIM14 init function */ void MX_TIM14_Init(void) { /* USER CODE BEGIN TIM14_Init 0 */ /* USER CODE END TIM14_Init 0 */ TIM_OC_InitTypeDef sConfigOC = {0}; /* USER CODE BEGIN TIM14_Init 1 */ /* USER CODE END TIM14_Init 1 */ htim14.Instance = TIM14; htim14.Init.Prescaler = 3; htim14.Init.CounterMode = TIM_COUNTERMODE_UP; htim14.Init.Period = 1000; htim14.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim14.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; if (HAL_TIM_Base_Init(&htim14) != HAL_OK) { Error_Handler(); } if (HAL_TIM_PWM_Init(&htim14) != HAL_OK) { Error_Handler(); } sConfigOC.OCMode = TIM_OCMODE_PWM1; sConfigOC.Pulse = 0; sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH; sConfigOC.OCFastMode = TIM_OCFAST_DISABLE; if (HAL_TIM_PWM_ConfigChannel(&htim14, &sConfigOC, TIM_CHANNEL_1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM14_Init 2 */ /* USER CODE END TIM14_Init 2 */ HAL_TIM_MspPostInit(&htim14); }
View more

Below are some functions being used to start PWM instances and update pulse widths. These functions work for all PWM instances not on TIM13 or TIM14 so far

//Called directly after generated inits for each instance and channel void Pwm_Instance_Start(TIM_HandleTypeDef *htim, uint32_t channel) { HAL_TIM_PWM_Start(htim, channel); } //Called in Freertos tasks to update LED brightness. //These calls are wrapped in mutexesto prevent faults void Update_Pwm_Duty_Cycle(uint16_t new_pulse_width, TIM_HandleTypeDef *htim, uint32_t channel) { TIM_OC_InitTypeDef sConfigOC = {0}; sConfigOC.OCMode = TIM_OCMODE_PWM1; sConfigOC.Pulse = new_pulse_width; sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH; sConfigOC.OCFastMode = TIM_OCFAST_DISABLE; if (HAL_TIM_PWM_ConfigChannel(htim, &sConfigOC, channel) != HAL_OK) { Error_Handler(); } }


 Let me know what other information/code may be helpful as well!

waclawek.jan
Super User

As @Tesla DeLorean said above, read out and post TIM and related GPIO and RCC registers content.

JW

Hi, apologies for the delayed response. Attached is a ZIP with photos of some of the register values I captured during some testing. Let me know if other specific registers at specific times would be useful to see.


waclawek.jan
Super User

These look OK.

Can you please check/post also the relevant GPIO registers content.

JW

Hi, apologies again for a late response. Here is the register values for GPIO port D.

dlewis_0-1745434166789.png

 

waclawek.jan
Super User

According to the STM32H562 datasheet, there is no TIM13 nor TIM14 pin at GPIOD.

JW

My apologies, I was looking at the port for the wrong PWM peripheral pin I was using. Here is the port values for GPIOA which should be the correct port.

dlewis_0-1745949796380.png

 

CMYL
ST Employee

Hello @dlewis 

In your configuration you missed to assign a value to pulse

sConfigOC.Pulse = 0; // in your settings sConfigOC.Pulse = 20; // for example

 PWM signal frequency is determined by the value of the TIMx_ARR register and a duty cycle determined by the value of the TIMx_CCRx register. The later takes the value of pulse parameter. It must be non zero otherwise no signal outputs.

/* Set the Capture Compare Register value */ TIMx->CCR1 = OC_Config->Pulse;

This is a test involving TIM13, TIM14 and TIM1 channel 1.

CMYL_0-1746023727721.png

Best Regards

Younes