User Activity

Hi All,I have a project that is using the STM32H562. I am having an issue using tim13 and tim14 to generate PWM outputs going to LEDs. The project uses timers tim2, tim3, tim4, tim13, and tim14 for a range of different PWM peripherals. For all of the...
Hi All,I am working on a project in CubeIDE workspace 1.17.0 and am having issues with my custom application source files not being indexed properly. My new files are being included in the build properly and the code from them is running, but the fil...