cancel
Showing results for 
Search instead for 
Did you mean: 

The pwm is generating ramp signals when using sensor with i2c interface

ShriyogJambekar
Associate

hello everyone, I am trying to combine a H-bridge-based motor controller and a sensor connected by i2c with stm32g032k8txx. They both work when i run on different microcontrollers, but when I combine them, the sensor is working fine but the PWM of the STM32 gets abnormal, like the output is something like a ramp signal (the motor initially starts at a slow speed and gradually increases to a high speed and stops. After some time, it starts again). Please help me if anyone knows about this problem.

3 REPLIES 3
SofLit
ST Employee

Hello,

You need to provide more details about your HW/Schematics it could be a conflicting HW ressources. If you're using CubeMx share your .ioc file.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

@SofLit i have attached the ioc file of the project so please check

You need to check your HW before going to check the Software.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.