cancel
Showing results for 
Search instead for 
Did you mean: 

the circuit of STM32F429 NRST

Zhang2024
Visitor

Hi all,

I'm using STM32F429BIT6。

my question is: C3 is 3.3uF±10%,How do you like this circuit?When WDG reset in the MCU  STM32F429BIT6,It will lead to CMOS failure of the MCU NRST?If C3 is 2.2uF±10%,the CMOS of the MCU NRST will be OK?Thanks!

NRST CircuitNRST CircuitWDG ResetWDG Reset

 

2 REPLIES 2
KnarfB
Principal III

Compare to the reference schematics in 

AN4488
Application note
Getting started with STM32F4xxxx MCU hardware development

hth

KnarfB

TDK
Guru

It will be fine, but the recommendation is to remove R5 since there is an internal pullup, and change C3 to a 0.1 uF.

TDK_0-1723298331461.png

dm00115714-getting-started-with-stm32f4xxxx-mcu-hardware-development-stmicroelectronics.pdf

If you feel a post has answered your question, please click "Accept as Solution".