2018-09-23 01:39 AM
hello
i am using stm32f103 for reading a 10 adc channels and i am using Dual mode regular simultaneous with DMA , the result are loaded in a buffer.
the problem is the loaded data from the ADC1 are in the right order (1st data is from 1st channel)
but the data from ADC2 are in the right sequence , for example : the last register in the buffer array is corresponding to the rank 3 of ADC2
how i can fix this
2018-09-23 09:09 AM
You know you could have just edited your original post/question.
Not using CubeMX+HAL+F1 combination here.
Couple of observations about F1:
Should not enable DMA until after calibration.
If lighting off another transfer in the callback consider using continuous mode, with circular DMA, with a double size buffer, managed the the DMA HT and TC interrupt/callback to manage in the inactive half.
The samples should be in interleaving pairs. With 5 samples on each it is going to be calling the IRQ a lot.
Don't view this functionality in the debugger. If you want to observe output values, use a non-volatile buffer and print to terminal. Or record much larger datasets.
Have previously post SPL examples
2018-09-23 10:17 AM
I had tried the same code without the callibration of the ADC, same problem appears,and also iam not using the adc in continuous mode, i make trigger after each DMA callback.
So why do you think that the saples of the adc2 overlaped.
Thanks for your help
2018-09-23 11:01 AM
>>and also iam not using the adc in continuous mode, i make trigger after each DMA callback.
Yes, I know, I wouldn't do that.
>>So why do you think that the samples of the adc2 overlapped.
How are you inspecting/logging this data?
2018-09-23 11:04 AM
>>>How are you inspecting/logging this data?
the adc buffer in initialized as volatile uint16_t monitored using st-link debugger.
2018-09-23 11:20 AM
I said this earlier "Don't view this functionality in the debugger. If you want to observe output values, use a non-volatile buffer and print to terminal. Or record much larger datasets."
2018-09-23 11:27 AM
i had tried also to print the values to treminal ,same result.
its really strange the values sampled by the adc1 are in right sequence , and the samples from the adc2 are not.
the steps that i am doing is :
in main function :
1-HAL_ADC_Start(&hadc2);
2-HAL_ADCEx_MultiModeStart_DMA(&hadc1,(uint32_t*)adc_buff,5);
in HAL_ADC_ConvCpltCallback function :
1-HAL_ADCEx_MultiModeStart_DMA(&hadc1,(uint32_t*)adc_buff,5);
am i missing anything?
2018-09-24 01:22 AM
I don't do Cube/HAL either.
With multi-channel ADC and DMA, I used validate the setup the following way:
- Set consecutively on ADC channel to about 1.5 .. 3.0V, the others to GND.
- Set a breakpoint in the DMA TC routine.
- Check the values of the channels.
- Swap the channel setup.
2018-09-24 01:39 AM
thanks for your help AvaTAr , but still not having solution 🙂
the result sampled from adc1 are loaded in correct order in the buffer ,
but the result from adc2 are not .
i dont know why , maybe some ovelapping , as i know the adc data of ADC1 and ADC2 are loaded in same register after a complete conversion , so i dont know what happen when the DMA load these value into variable array,and why only the data of ADC2 are not in sequence,
2018-09-24 02:24 AM
I don't know what Cube/HAL is doing here, and honestly, my trust is limited.
I suggest to check the initialization code, and compare the result (the ADC config register settings) with the expected values, reading the reference manual.
I used the ADC a lot (with SPL / register code), and never had such problems.