2022-07-26 4:00 AM
Hello, I'm trying to implement the temperature sensor TSYS01 on STM32U575I-EV.
The datasheet of the sensor tells to reset the sensor first so I'm trying to do this like this:
HAL_I2C_Master_Transmit(&hi2c2, 0x77 << 1, 0x1E, 1, HAL_MAX_DELAY);0x77 << 1 - sensor address
0x1E - reset address.
After executing this command the board fails into HardFault_Handler.
I also tried to use the code from this repository, but also no success github: eddyem/tsys01
Here I found generic driver: github: TEConnectivity/TSYS01_Generic_C_Driver
Please, help.
Thank you.
2022-07-26 5:17 AM
Doesn't it expect a pointer?