cancel
Showing results for 
Search instead for 
Did you mean: 

SWD Pins on STM32L476RG

SSaha.1
Associate III

Instead of using JTAG, I would like to enable SWD programming (via STLink) for a custom STM32L476RG board that I am designing. Which pins of the MCU correspond to the 5 SWD pins normally found on boards like Nucleo and Sensortile? I probably found out 4 of the 5 pins (VDD, GND, NRST (reset) and SWDIO (PA13)) but can't find SWDCLK.

2 REPLIES 2

PA13 (SWDIO), PA14 (SWCLK), PB3 (SWO), NRST, GND

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TDK
Guru

SWCLK is PA14.

Can be found in the reference manual, the datasheet, STM32CubeMX and other places.

If you feel a post has answered your question, please click "Accept as Solution".