2025-02-12 5:34 AM
Hi!
I have a custom STM32H753ZIT6 MCU based board for which I am using SWD in order to bootload/program the MCU. To interface the SWD to either the STLINK or other programming modules similar to it, does anyone have any recommendation on what connect to use. From my research I have seen TC2030 being used in few designs but that is fairly expensive connector to interface with STLINK. Do you have any recommendation on what connector I could incorporate in my designs. I had an idea to have 10 pin female header connector with similar pitch to what stlink has as I observed the pinouts for SWD are on one side of 20 pin connector, could be a *** idea, if you have some better alternative please recommend.
Solved! Go to Solution.
2025-02-12 7:40 AM
Use a standard shrouded header that mates with the cable on your programmer. Either 0.1" or 0.05" pitch depending on your programmer.
For STLINK-V3MINIE, use Samtec FTSH-107-01-F-DV-K or equivalent and use the standard pinout.
2025-02-12 7:40 AM
Use a standard shrouded header that mates with the cable on your programmer. Either 0.1" or 0.05" pitch depending on your programmer.
For STLINK-V3MINIE, use Samtec FTSH-107-01-F-DV-K or equivalent and use the standard pinout.
2025-02-12 7:48 AM
You can use whatever connector you find convenient - or even no actual connector at all!
ARM's standard recommendation: https://documentation-service.arm.com/static/5fce6c49e167456a35b36af1
A "no-connector" example: https://www.tag-connect.com/
But do be sure to include NRST - that can get you out of some "stuck" conditions ...
2025-02-13 1:23 PM - edited 2025-02-13 1:24 PM
TAG-connect is cool but too expensive. Some ST eval boards for STM32C0 come with a white plastic connector that fits on the edge of the board and the ST-LINK MINIE on the other end. I never can remember the name of this thing.
On the board you just make 4 metallized strips on any edge. The ST-LINK MINIE has similar strips. No pins, holes or soldering.