2017-03-21 4:47 AM
When I try to run and debug a project with SW4STM32-Eclipse I get the following error message:
Error in final launch sequence
Failed to execute MI command:
-exec-run
Error message from debugger back end:
Don't know how to run. Try 'help target'.
Any suggestion?
Luca
2017-03-22 8:27 AM
Hello,
Which version of SW4STM32/eclipse are you using ? Ensure that you are using the updated version.
Imen
2017-03-22 8:34 AM
Hi Imen,
Eclipse: 20160218-0600 (Version Mars.2 Release 4.5.2)
SW4STM: 1.13.1.201701261206
Luca
2017-04-28 6:57 AM
Hello Luca,
Could you describe a bit more your env ?
What is your host OS ?
Which project are you trying to build and upload into the which SoC ?
If you are trying an example, which one ?
Have you installed all neccessary drivers for Win, or necessary libs for Linux/Mac ?
Kind regards
Sirma