cancel
Showing results for 
Search instead for 
Did you mean: 

SW4STM32 + STM32F411E Disco

Luca R
Associate II
Posted on March 21, 2017 at 12:47

When I try to run and debug a project with SW4STM32-Eclipse I get the following error message:

Error in final launch sequence

Failed to execute MI command:

-exec-run

Error message from debugger back end:

Don't know how to run. Try 'help target'.

Any suggestion?

Luca

3 REPLIES 3
Imen.D
ST Employee
Posted on March 22, 2017 at 16:27

Hello,

Which version of SW4STM32/eclipse are you using ? Ensure that you are using the updated version.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Luca R
Associate II
Posted on March 22, 2017 at 16:34

Hi Imen,

Eclipse: 20160218-0600 (Version Mars.2 Release 4.5.2)

SW4STM: 1.13.1.201701261206

Luca

Sirma Siang
ST Employee
Posted on April 28, 2017 at 15:57

Hello Luca,

Could you describe a bit more your env ?

What is your host OS ?

Which project are you trying to build and upload into the which SoC ?

If you are trying an example, which one ?

Have you installed all neccessary drivers for Win, or necessary libs for Linux/Mac ?

Kind regards

Sirma