cancel
Showing results for 
Search instead for 
Did you mean: 

Suspected error in STM32F334X8_FLASH.ld in STM32CubeF3 1.3

carmine
Associate II
Posted on September 26, 2015 at 08:02

Hi,

After struggling trying to make a Nucleo-F334R8 working with the latest HAL, I reached to the conclusion that the linker script shipped with the HAL is wrong. The memory sections are defined as follow:

/* Highest address of the user mode stack */

_estack = 0x20003FFF; /* end of RAM */

/* Generate a link error if heap and stack don't fit into RAM */

_Min_Heap_Size = 0x200; /* required amount of heap */

_Min_Stack_Size = 0x400; /* required amount of stack */

/* Specify the memory areas */

MEMORY

{

FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 64K

RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 16K

CCMRAM (rw) : ORIGIN = 0x10000000, LENGTH = 4K

}

But this script lead to a BusFault error, as STM32F334R8 has 12KB SRAM + 4KB CCM. So, changing the linker script in the following way solves the problem:

/* Entry Point */

ENTRY(Reset_Handler)

/* Highest address of the user mode stack */

_estack = 0x20003000; /* end of RAM */

/* Generate a link error if heap and stack don't fit into RAM */

_Min_Heap_Size = 0x200; /* required amount of heap */

_Min_Stack_Size = 0x400; /* required amount of stack */

/* Specify the memory areas */

MEMORY

{

FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 64K

RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 12K

CCMRAM (rw) : ORIGIN = 0x10000000, LENGTH = 4K

}

If I'm wrong, please explain me why the second link script works :)

#stm32f334-nucleo-bus-fault

2 REPLIES 2
Nesrine M_O
Lead II
Posted on September 28, 2015 at 12:05

Hi cnoviello,

I will check this problem with our development team & come back to you.Sorry for the inconvenience that it may bring.

-Syrine-

Nesrine M_O
Lead II
Posted on September 28, 2015 at 16:30

Hi cnoviello,

You are right. Thank you for bringing this issue to our attention.

It is noted and will be fixed in coming release of the STM32cubeF3 package.

-Syrine-