2024-11-20 9:01 PM - last edited on 2024-11-21 1:50 AM by Andrew Neil
Hi everyone,
I'm trying to support a 2TB SDXC using the STM32F407 microchip as a data logger. However, I encountered an issue where only around 220GB of memory can be formatted properly, instead of the full 2TB capacity.
I suspected there might be a limitation in the file system(might be the lenth of a pointer or something) that restricts the addressable memory size. I've tried to trace back through the file system code but haven't been able to access the low-level implementation that might be causing this problem,
Has anyone encountered similar issues or could provide some insights on:
1. How to properly implement SDXC card support for large capacities?
2. Any specific modifications needed in the file system to handle >1TB storage?
Any help or guidance would be greatly appreciated.
2024-11-20 10:13 PM
Would need to be a legitimate card
Probably going to need to use a more current version of FatFS and EXFAT format.
Certainly should be possible to support 400 or 512 GB cards, although those a heading toward unpractically large based on the caching and file system structures