Strangest problem ever seen - Specific value in flash causes DMA underrun. Any ideas?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-06 7:33 AM
I have the strangest problem ever seen and I would not believe it has it not been this repeatable:
I have a single DMA controller running 3x streams. Two are for ADC and one for DAC. All three can run simultaneously, the DAC at 1 Msps and the ADCs both at 40 ksps with the ADC DMA only constantly and the DAC DMA running for about 1 second on command.
After implementing our embedded loader that writes to flash, I started getting DMA FIFO errors on the DAC stream.
After A LOT of trial-and-error I found that when the word at address 0x0810000C was programmed, then I would see this problem. The rest of the flash in sector 8 is still erased.
The following process is 100% repeatable, even on different boards (same CPU, different IO configuration, same code):
- Use STM32CubeProgramer for all steps below.
- Check that entire sector 8 is erased (all 0xFFFFFFFF).
- Write flash @0x0810000C with 0x08000000.
- Perform Hard reset and run.
- Perform a DMA access on DAC while ADC stream running.
- Triggers a FIFO error on DAC stream.
- I can now repeat steps 4 and 5 above and consistently get the same result.
- Write flash @0x0810000C with 0xFFFFFFFF.
- Perform Hard reset and run.
- Perform a DMA access on DAC while ADC stream running.
- DAC DMA transfer completes normally.
- I can now repeat steps 9 and 10 and consistently get the same results but I can also repeat steps 1 to 11 and consistently get the same results.
I've used a hardware breakpoint to make sure none of my code ever access flash in sector 8.
It gets stranger: To check that my hardware breakpoint was set correctly, I wrote some test code to read @0x0810000C. This worked, but when I programmed my board a second time it would not come out of reset. Again, I had a VERY LONG investigation. The RESET pin on my board was toggling at 13 kHz and the debugger would in no way re-connect.
My solution was to change my BOOT0 pin from low to high so that my test code would never execute. I could then use the CLI of the cube programmer (neither the IDE nor GUI worked) to do a mass erase ONLY when I did not connect under reset. This managed to recover the board.
Any idea why this flash address is special? I have considered that I may have erroneous code but my code runs flawlessly for days on end until I write that one flash address. Not all values work. Writing it to all zero, 0xA5A5A5A5 would not cause the same problem.
- Labels:
-
DAC
-
DMA
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-06 7:49 AM
Include your chip number. There are thousands of different STM32 parts.
> The RESET pin on my board was toggling at 13 kHz and the debugger would in no way re-connect.
Indicates the chip is resetting itself. Examine SCB->CSR to determine why.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-06 8:03 AM
There is some reason why you write various values to flash @0810000C, so I assume this value is used somewhere else in your program, and that's what causes your problem.
Reduce your program by removing features and observe when does the problem disappear.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-06 11:38 AM
I am using STM32H745.
When I was in this last state (where chip kept on resetting itself) I could not examine CSR because I could not connect to the CPU.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-06 11:41 AM
I am using bank 1 when upgrading software and swopping the banks after download is complete. This is how I originally found my problem: It would only occur on boards that has been programmed, so it had data written in bank 1 of Flash. I never read that memory. It is only written when doing software upgrade.
It is through reducing functionality that I found that only that one specific address has a role to play. I agree most reasonable cause is something in my code changing because of that value being written but my code does not use it.
I am hoping that someone knows that the ROM code may be using it prior to my code even running?