cancel
Showing results for 
Search instead for 
Did you mean: 

Store values in STM32G0 internal flash

Himanshu Saxena
Associate II

(was initially a reply to https://community.st.com/t5/stm32-mcus-products/store-values-in-internal-flash/m-p/666974

 

I am store variable in flash adders and after reset read but variable values is not store in flash adders.& using stm32g030f6p6 microcontroller and here is my code:-

void flash unlock(void)

{

 FLASH->KEYR = 0x45670123;

 FLASH->KEYR = 0xCDEF89AB;

}

 

 

void Erase_Flash(void)

{

 //HRTIM1->sMasterRegs.MICR |= 0x51;  /*clear pending bit*/

 // HRTIM1->sMasterRegs.MDIER = HRTIM_MASTER_IT_NONE; /*DISABLE HRTIMER INTERRUPT*/

  

  flash_unlock();

   Delay(200); 

 /*if((FLASH->CR &0x80)== 0x80)

 {

  flash_unlock();

  delay2(200);

 }

  

  

 else*/

 {

  SET_BIT(FLASH->CR, FLASH_CR_PER);  

    Delay(200); 

  FLASH->WRP1AR = 0x08000500;

    Delay(200); 

  FLASH->CR |= 0x40;

  FLASH->WRP1AR = 0x08000800;

    Delay(200); 

  FLASH->CR |= 0x40;

  /* FLASH->WRP1AR = 0x08007C10;

    Delay(200); 

  FLASH->CR |= 0x40;

  FLASH->WRP1AR = 0x08007C14;

    Delay(200); 

  FLASH->CR |= 0x40;

    Delay(200); */

  CLEAR_BIT(FLASH->CR, FLASH_CR_PER);   

 } 

 // HRTIM1->sMasterRegs.MDIER = HRTIM_MDIER_MUPDIE;  /*ENABLE HRTIMER INTERRUPT*/ 

 

void flash_write(void)

{

 // HRTIM1->sMasterRegs.MICR |= 0x51;  /*clear pending bit*/

 // HRTIM1->sMasterRegs.MDIER = HRTIM_MASTER_IT_NONE; /*DISABLE HRTIMER INTERRUPT*/

 Erase_Flash();   

 //HRTIM1->sMasterRegs.MICR |= 0x51;  /*clear pending bit*/

 //HRTIM1->sMasterRegs.MDIER = HRTIM_MASTER_IT_NONE; /*DISABLE HRTIMER INTERRUPT*/

 /*if((FLASH->CR &0x80)== 0x80)

 {

  flash_unlock();

  delay2(200);

 }

 else*/

 {

  //flash_unlock();

    Delay(10000); 

  SET_BIT(FLASH->CR, FLASH_CR_PG);  

    Delay(10000); 

  *(__IO uint16_t*)0x08000500 = 596; ///PV_cal

    Delay(10000); 

  *(__IO uint16_t*)0x08000800 = 456; ///BV_cal

    Delay(10000); 

 /* *(__IO uint16_t*)0x08007C10 = VAR3; //BI_cal

    Delay(10000); 

  *(__IO uint16_t*)0x08007C14 = VAR4; //Induct_cal

    Delay(10000); 

  *(__IO uint16_t*)0x08007C18 = VAR5; //Induct_cal

    Delay(10000); 

  // *(__IO uint16_t*)0x08007C1C = 0xAD; //first time

   Delay(10000); */

  CLEAR_BIT(FLASH->CR, FLASH_CR_PG);  

 }  

 // HRTIM1->sMasterRegs.MDIER = HRTIM_MDIER_MUPDIE;  /*ENABLE HRTIMER INTERRUPT*/  

}

 

 

void flash(void)

 {  

 VAR1  = *(__IO uint16_t*)0x08000500;

  Delay(20); 

 VAR2  = *(__IO uint16_t*)0x08000800;

  Delay(20); 

 /* VAR3  = *(__IO uint16_t*)0x08007C10;

  Delay(20); 

 VAR4 = *(__IO uint16_t*)0x08007C14;

  Delay(20); 

  VAR5 = *(__IO uint16_t*)0x08007C18;

  Delay(20); 

  //First = *(__IO uint16_t*)0x08007C1C;

   Delay(20); */

}

1 ACCEPTED SOLUTION

Accepted Solutions

Use </> code formatting tool to post source code.

Add comments

Does library code work? Low addresses likely to contain the executing code, can't just erase 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

4 REPLIES 4

Use </> code formatting tool to post source code.

Add comments

Does library code work? Low addresses likely to contain the executing code, can't just erase 

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TDK
Super User

It looks like you're trying to erase individual sections of flash, but your code is misguided and won't work. Perhaps go from a HAL example.

Look at how flash operates--particularly that you can only erase an entire sector at a time.

Also note that erasing flash that is currently in use by the program will cause your program to stop working.

If you feel a post has answered your question, please click "Accept as Solution".
void flash unlock(void)
{
 FLASH->KEYR = 0x45670123;
 FLASH->KEYR = 0xCDEF89AB;
}
void Erase_Flash(void)
{   flash_unlock();
   Delay(200); 
 /*if((FLASH->CR &0x80)== 0x80)
 {
  flash_unlock();
  delay2(200);
 }
 else*/
 {
  SET_BIT(FLASH->CR, FLASH_CR_PER);  
    Delay(200); 
  FLASH->WRP1AR = 0x08000500;
    Delay(200); 
  FLASH->CR |= 0x40;
  FLASH->WRP1AR = 0x08000800;
    Delay(200); 
  FLASH->CR |= 0x40;
  /* FLASH->WRP1AR = 0x08007C10;
    Delay(200); 
  FLASH->CR |= 0x40;
  FLASH->WRP1AR = 0x08007C14;
    Delay(200); 
  FLASH->CR |= 0x40;
    Delay(200); */
  CLEAR_BIT(FLASH->CR, FLASH_CR_PER);   
 } 
 } 
 
void flash_write(void)
{
  Erase_Flash();   
 /*if((FLASH->CR &0x80)== 0x80)
 {
  flash_unlock();
  delay2(200);
 }
 else*/
 {
  //flash_unlock();
    Delay(10000); 
  SET_BIT(FLASH->CR, FLASH_CR_PG);  
    Delay(10000); 
  *(__IO uint16_t*)0x08000500 = 596; ///PV_cal
    Delay(10000); 
  *(__IO uint16_t*)0x08000800 = 456; ///BV_cal
    Delay(10000); 
 /* *(__IO uint16_t*)0x08007C10 = VAR3; //BI_cal
    Delay(10000); 
  *(__IO uint16_t*)0x08007C14 = VAR4; //Induct_cal
    Delay(10000); 
  *(__IO uint16_t*)0x08007C18 = VAR5; //Induct_cal
    Delay(10000); 
  // *(__IO uint16_t*)0x08007C1C = 0xAD; //first time
   Delay(10000); */
  CLEAR_BIT(FLASH->CR, FLASH_CR_PG);  
 }  
 }
 void flash(void)
 {  
 VAR1  = *(__IO uint16_t*)0x08000500;
  Delay(20); 
 VAR2  = *(__IO uint16_t*)0x08000800;
  Delay(20); 
 /* VAR3  = *(__IO uint16_t*)0x08007C10;
  Delay(20); 
 VAR4 = *(__IO uint16_t*)0x08007C14;
  Delay(20); 
  VAR5 = *(__IO uint16_t*)0x08007C18;
  Delay(20); 
  //First = *(__IO uint16_t*)0x08007C1C;
   Delay(20); */
}

yes when i am erase flasg entire program is stop working , may be my flash adders is not correct or correct ,please refer any addears to replace it.