cancel
Showing results for 
Search instead for 
Did you mean: 

STMP32H7 UART1 RS422 DMA Rx not functioning but Tx works.

CWang.16
Associate

Have STPM32H7 CPU running in 108 Mhz, and UART1 pull off PLL3 @50 Mhz, set baud rate at 3375000 with 8x oversampling rate.

Do see the Tx signal by DMA (303 ns each baud ) out to device and replied with about 302 ns baud, signal is clean on the scope, however, the DMA Rx never catch anything. Both are working fine when it is half the baud rate( 1687500 with 16x oversampling ).

What else need to change for DMA Rx?

0 REPLIES 0