cancel
Showing results for 
Search instead for 
Did you mean: 

How can you enable TouchGFX within STMCube, using only internal memory (no FMC SDRAM)?

sasha
Associate III

I want to create a project using an STM32F7 core, but don't want external memory - the MCU has more than enough memory for one or even two framebuffers in internal RAM. However - STMCube will not allow me to enable the Graphics Framework without FMC enabled. Is there away around this?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Shahrear
Associate II

yes. its possible