2023-03-16 7:35 AM
Hi, I am using an STM32F401CCU6 for a FreeRTOS project. My problem is that a variable shows up in the Build Analyzer as 64B instead of 80B.
I am using some LoRa libraries. For simplicity, I will refer only to the information I think is relevant for the problem.
-- I have a type called lora_status_t defined as follows:
typedef struct {
uint8_t opmode;
uint8_t version;
uint8_t sync_word;
// pa config
uint8_t pa_config;
uint8_t pa_select;
float max_power;
float output_power_dbm;
// modem config 1
uint8_t modem_config_1;
float bw;
uint8_t implicit;
float coding_rate;
// modem config 2
uint8_t modem_config_2;
uint16_t spreading_factor;
uint8_t tx_continuous_mode;
uint8_t rx_payload_crc_on;
// modem config 3
uint8_t modem_config_3;
// Lora Page registers
uint8_t fifoAddrPtr;
uint8_t fifoTxBaseAddr;
uint8_t fifoRxBaseAddr;
uint8_t fifoRxCurrAddr;
uint8_t fifoRxBytesNb;
uint16_t validHeaderCnt;
uint16_t validPacketCnt;
} lora_status_t;
-- I have another type, lora_sx127x which contains some variables, including one lora_status_t.
// LORA definition
typedef struct {
// SPI parameters
SPI_HandleTypeDef *spi;
GPIO_TypeDef *nss_port;
uint32_t spi_timeout;
// Operating frequency, in Hz
uint32_t frequency;
// Output PIN (module internal, not related to your design)
// Can be one of PA_OUTPUT_PA_BOOST / PA_OUTPUT_RFO
uint32_t pa_mode;
// Base FIFO addresses for RX/TX
uint8_t tx_base_addr;
uint8_t rx_base_addr;
uint16_t nss_pin;
GPIO_TypeDef *reset_port;
uint16_t reset_pin;
lora_status_t status;
} lora_sx127x;
-- sizeof(lora_status_t) = 48
-- sizeof(lora_sx127x) = 80
Buil Analyzer instead shows it as 68B. This means all debugging using STMCubeIDE in that zone is lacking 12B, which means, for example, that Live Expressions of expressions right after the (lora_sx127x)lora variable show wrong values.
Build Analyzer, under .bss:
This is an extraction of the .map generated from the Debug:
...
.bss.xIdleTaskTCBBuffer
0x00000000200011a8 0xb4 ./Core/Src/freertos.o
.bss.xIdleStack
0x000000002000125c 0x200 ./Core/Src/freertos.o
.bss.lora 0x000000002000145c 0x50 ./Core/Src/main.o
0x000000002000145c lora
.bss.hrtc 0x00000000200014ac 0x20 ./Core/Src/rtc.o
0x00000000200014ac hrtc
.bss.hspi1 0x00000000200014cc 0x58 ./Core/Src/spi.o
0x00000000200014cc hspi1
.bss.__sbrk_heap_end
0x0000000020001524 0x4 ./Core/Src/sysmem.o
.bss.uwTick 0x0000000020001528 0x4 ./Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal.o
0x0000000020001528 uwTick
...
It interesting that the .bss.lora variable is actually 0x50 = dec80 in size in the memory map! A curious thing is that I cannot find the variables changeDateTime_External_flag and changeDateTime_External_dateTime in the map file. I checked that the build analyzer shows the correct date and time of the elf file being analyzed.
Thanks for your time,
S.
Solved! Go to Solution.
2023-03-16 9:01 AM
I have solved the problem. There was another header being included before the definition of the LoRa libraries. This header contained #pragma pack(1) without at #pragma pack(4) at the end. Adding a #pragma pack(4) at the end of that header fixed the problem.
Open questions:
2023-03-16 9:01 AM
I have solved the problem. There was another header being included before the definition of the LoRa libraries. This header contained #pragma pack(1) without at #pragma pack(4) at the end. Adding a #pragma pack(4) at the end of that header fixed the problem.
Open questions:
2023-03-19 2:21 AM
I answer to myself again. According to ARM documentation, the pointer to an unaligned struct must be explicitly defined as one using the keyword __packed, otherwise the "->" will just not work:
"When a pointer is declared as __packed, the compiler generates code that correctly accesses the dereferenced value of the pointer, regardless of its alignment. The generated code consists of a sequence of byte accesses, or variable alignment-dependent shifting and masking instructions, rather than a simple LDR instruction. Consequently, declaring a pointer as __packed incurs a performance and code size penalty."