2018-02-22 3:55 PM
I am running version 4.24.0 of stm32cubeMX. I recently realized that when I try to generate any code the has rtc in it, the code generated in the rtc.c file is full of errors.
I have tried on both Mac OSX and Win 72018-02-22 11:39 PM
I would add some additional info:
-HAL or LL drivers?
-Target IDE - Keil, Atollic...?
-maybe ioc project file to see what was enabled
2018-02-26 4:10 AM
Hello
Gwena.Munyaradzi
,Could you please attach your ioc file to check your issue.
What exactly did the error message say?
Best Regards,Imen
2018-02-26 4:54 AM
Hi
Gwena.Munyaradzi
,I want to thank you for your bug report and posting the details.
This issue is raised internally in CubeMx team and will be fixed in the next CubeMX release.
Sorry for any inconvenience it may cause.
Kind Regards,
Imen
2018-02-26 4:57 AM
,
,
I'm using HAL the target IDE is System Workbench for STM32
,
♯ MicroXplorer Configuration settings - do not modify,
FREERTOS.IPParameters=Tasks01,
FREERTOS.Tasks01=defaultTask,0,128,StartDefaultTask,Default,NULL,
File.Version=6,
KeepUserPlacement=false,
Mcu.Family=STM32F1,
Mcu.IP0=FREERTOS,
Mcu.IP1=NVIC,
Mcu.IP2=RCC,
Mcu.IP3=RTC,
Mcu.IP4=SYS,
Mcu.IPNb=5,
Mcu.Name=STM32F103R(C-D-E)Tx,
Mcu.Package=LQFP64,
Mcu.Pin0=PA13,
Mcu.Pin1=VP_FREERTOS_VS_ENABLE,
Mcu.Pin2=VP_RTC_VS_RTC_Activate,
Mcu.Pin3=VP_RTC_VS_RTC_Calendar,
Mcu.Pin4=VP_SYS_VS_ND,
Mcu.Pin5=VP_SYS_VS_tim1,
Mcu.PinsNb=6,
Mcu.ThirdPartyNb=0,
Mcu.UserConstants=,
Mcu.UserName=STM32F103RCTx,
MxCube.Version=4.24.0,
MxDb.Version=DB.4.0.240,
NVIC.BusFault_IRQn=true\:0\:0\:false\:false\:true\:false\:false,
NVIC.DebugMonitor_IRQn=true\:0\:0\:false\:false\:true\:false\:false,
NVIC.HardFault_IRQn=true\:0\:0\:false\:false\:true\:false\:false,
NVIC.MemoryManagement_IRQn=true\:0\:0\:false\:false\:true\:false\:false,
NVIC.NonMaskableInt_IRQn=true\:0\:0\:false\:false\:true\:false\:false,
NVIC.PendSV_IRQn=true\:15\:0\:false\:false\:false\:true\:false,
NVIC.PriorityGroup=NVIC_PRIORITYGROUP_4,
NVIC.SVCall_IRQn=true\:0\:0\:false\:false\:false\:false\:false,
NVIC.SysTick_IRQn=true\:15\:0\:false\:false\:true\:true\:false,
NVIC.TIM1_UP_IRQn=true\:0\:0\:false\:false\:true\:false\:false,
NVIC.TimeBase=TIM1_UP_IRQn,
NVIC.TimeBaseIP=TIM1,
NVIC.UsageFault_IRQn=true\:0\:0\:false\:false\:true\:false\:false,
PA13.Locked=true,
PA13.Signal=GPIO_Output,
PCC.Checker=false,
PCC.Line=STM32F103,
PCC.MCU=STM32F103R(C-D-E)Tx,
PCC.PartNumber=STM32F103RCTx,
PCC.Seq0=0,
PCC.Series=STM32F1,
PCC.Temperature=25,
PCC.Vdd=3.3,
PinOutPanel.RotationAngle=0,
ProjectManager.AskForMigrate=true,
ProjectManager.BackupPrevious=false,
ProjectManager.CompilerOptimize=2,
ProjectManager.ComputerToolchain=false,
ProjectManager.CoupleFile=true,
ProjectManager.CustomerFirmwarePackage=C\:/Users/munya/.stm32cubemx/plugins/updater/STM32Cube_FW_F1_V1.6.0,
ProjectManager.DefaultFWLocation=true,
ProjectManager.DeletePrevious=true,
ProjectManager.DeviceId=STM32F103RCTx,
ProjectManager.FirmwarePackage=STM32Cube FW_F1 V1.6.0,
ProjectManager.FreePins=false,
ProjectManager.HalAssertFull=false,
ProjectManager.HeapSize=0x200,
ProjectManager.KeepUserCode=true,
ProjectManager.LastFirmware=true,
ProjectManager.LibraryCopy=1,
ProjectManager.PreviousToolchain=SW4STM32,
ProjectManager.ProjectBuild=false,
ProjectManager.ProjectFileName=MK11_RTC.ioc,
ProjectManager.ProjectName=MK11_RTC,
ProjectManager.StackSize=0x400,
ProjectManager.TargetToolchain=SW4STM32,
ProjectManager.ToolChainLocation=,
ProjectManager.UnderRoot=true,
ProjectManager.functionlistsort=1-MX_GPIO_Init-GPIO-false-HAL-true,2-SystemClock_Config-RCC-false-HAL-true,3-MX_RTC_Init-RTC-false-HAL-true,
RCC.APB1Freq_Value=8000000,
RCC.APB2Freq_Value=8000000,
RCC.FamilyName=M,
RCC.IPParameters=APB1Freq_Value,APB2Freq_Value,FamilyName,PLLCLKFreq_Value,PLLMCOFreq_Value,TimSysFreq_Value,
RCC.PLLCLKFreq_Value=8000000,
RCC.PLLMCOFreq_Value=4000000,
RCC.TimSysFreq_Value=8000000,
VP_FREERTOS_VS_ENABLE.Mode=Enabled,
VP_FREERTOS_VS_ENABLE.Signal=FREERTOS_VS_ENABLE,
VP_RTC_VS_RTC_Activate.Mode=RTC_Enabled,
VP_RTC_VS_RTC_Activate.Signal=RTC_VS_RTC_Activate,
VP_RTC_VS_RTC_Calendar.Mode=RTC_Calendar,
VP_RTC_VS_RTC_Calendar.Signal=RTC_VS_RTC_Calendar,
VP_SYS_VS_ND.Mode=No_Debug,
VP_SYS_VS_ND.Signal=SYS_VS_ND,
VP_SYS_VS_tim1.Mode=TIM1,
VP_SYS_VS_tim1.Signal=SYS_VS_tim1,
board=MK11_RTC2018-02-26 5:31 AM
Hi
DAHMEN.IMEN
Sorry I can't seem to be able to attach a file. I will have to send the the content of the ioc file.
#MicroXplorer Configuration settings - do not modify
FREERTOS.IPParameters=Tasks01 FREERTOS.Tasks01=defaultTask,0,128,StartDefaultTask,Default,NULL File.Version=6 KeepUserPlacement=false Mcu.Family=STM32F1 Mcu.IP0=FREERTOS Mcu.IP1=NVIC Mcu.IP2=RCC Mcu.IP3=RTC Mcu.IP4=SYS Mcu.IPNb=5 Mcu.Name=STM32F103R(C-D-E)Tx Mcu.Package=LQFP64 Mcu.Pin0=PA13 Mcu.Pin1=VP_FREERTOS_VS_ENABLE Mcu.Pin2=VP_RTC_VS_RTC_Activate Mcu.Pin3=VP_RTC_VS_RTC_Calendar Mcu.Pin4=VP_SYS_VS_ND Mcu.Pin5=VP_SYS_VS_tim1 Mcu.PinsNb=6 Mcu.ThirdPartyNb=0 Mcu.UserConstants= Mcu.UserName=STM32F103RCTx MxCube.Version=4.0 MxDb.Version=DB.4.0.240 NVIC.BusFault_IRQn=true\:0\:0\:false\:false\:true\:false\:false NVIC.DebugMonitor_IRQn=true\:0\:0\:false\:false\:true\:false\:false NVIC.HardFault_IRQn=true\:0\:0\:false\:false\:true\:false\:false NVIC.MemoryManagement_IRQn=true\:0\:0\:false\:false\:true\:false\:false NVIC.NonMaskableInt_IRQn=true\:0\:0\:false\:false\:true\:false\:false NVIC.PendSV_IRQn=true\:15\:0\:false\:false\:false\:true\:false NVIC.PriorityGroup=NVIC_PRIORITYGROUP_4 NVIC.SVCall_IRQn=true\:0\:0\:false\:false\:false\:false\:false NVIC.SysTick_IRQn=true\:15\:0\:false\:false\:true\:true\:false NVIC.TIM1_UP_IRQn=true\:0\:0\:false\:false\:true\:false\:false NVIC.TimeBase=TIM1_UP_IRQn NVIC.TimeBaseIP=TIM1 NVIC.UsageFault_IRQn=true\:0\:0\:false\:false\:true\:false\:false PALocked=true PASignal=GPIO_Output PCC.Checker=false PCC.Line=STM32F103 PCC.MCU=STM32F103R(C-D-E)Tx PCC.PartNumber=STM32F103RCTx PCC.Seq0=0 PCC.Series=STM32F1 PCC.Temperature=25 PCC.Vdd=3.3 PinOutPanel.RotationAngle=0 ProjectManager.AskForMigrate=true ProjectManager.BackupPrevious=false ProjectManager.CompilerOptimize=2 ProjectManager.ComputerToolchain=false ProjectManager.CoupleFile=true ProjectManager.CustomerFirmwarePackage=C\:/Users/munya/.stm32cubemx/plugins/updater/STM32Cube_FW_F1_V1.6.0 ProjectManager.DefaultFWLocation=true ProjectManager.DeletePrevious=true ProjectManager.DeviceId=STM32F103RCTx ProjectManager.FirmwarePackage=STM32Cube FW_F1 V1.6.0 ProjectManager.FreePins=false ProjectManager.HalAssertFull=false ProjectManager.HeapSize=0x200 ProjectManager.KeepUserCode=true ProjectManager.LastFirmware=true ProjectManager.LibraryCopy=1 ProjectManager.PreviousToolchain=SW4STM32 ProjectManager.ProjectBuild=false ProjectManager.ProjectFileName=MK11_RTC.ioc ProjectManager.ProjectName=MK11_RTC ProjectManager.StackSize=0x400 ProjectManager.TargetToolchain=SW4STM32 ProjectManager.ToolChainLocation= ProjectManager.UnderRoot=true ProjectManager.functionlistsort=1-MX_GPIO_Init-GPIO-false-HAL-true,2-SystemClock_Config-RCC-false-HAL-true,3-MX_RTC_Init-RTC-false-HAL-true RCC.APB1Freq_Value=8000000 RCC.APB2Freq_Value=8000000 RCC.FamilyName=M RCC.IPParameters=APB1Freq_Value,APB2Freq_Value,FamilyName,PLLCLKFreq_Value,PLLMCOFreq_Value,TimSysFreq_Value RCC.PLLCLKFreq_Value=8000000 RCC.PLLMCOFreq_Value=4000000 RCC.TimSysFreq_Value=8000000 VP_FREERTOS_VS_ENABLE.Mode=Enabled VP_FREERTOS_VS_ENABLE.Signal=FREERTOS_VS_ENABLE VP_RTC_VS_RTC_Activate.Mode=RTC_Enabled VP_RTC_VS_RTC_Activate.Signal=RTC_VS_RTC_Activate VP_RTC_VS_RTC_Calendar.Mode=RTC_Calendar VP_RTC_VS_RTC_Calendar.Signal=RTC_VS_RTC_Calendar VP_SYS_VS_ND.Mode=No_Debug VP_SYS_VS_ND.Signal=SYS_VS_ND VP_SYS_VS_tim1.Mode=TIM1 VP_SYS_VS_tim1.Signal=SYS_VS_tim1 board=MK11_RTC2018-02-26 5:32 AM
DAHMEN.IMEN
the Generated rtc.c file has this in it:
/* Includes ------------------------------------------------------------------*/
#include 'rtc.h' #n#n
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
RTC_HandleTypeDef hrtc;
#n /* RTC init function */ void MX_RTC_Init(void) { #tRTC_TimeTypeDef sTime; #tRTC_DateTypeDef DateToUpdate; #n #t#t/**Initialize RTC Only #n#t#t*/ #thrtc.Instance = RTC; #tif(HAL_RTCEx_BKUPRead(&hrtc, RTC_BKP_DR1) != 0x32F2){ #thrtc.Init.AsynchPrediv = RTC_AUTO_1_SECOND; #thrtc.Init.OutPut = RTC_OUTPUTSOURCE_ALARM; #tif (HAL_RTC_Init(&hrtc) != HAL_OK) #t{ #t#t_Error_Handler(__FILE__, __LINE__); #t} #n #t#t/**Initialize RTC and set the Time and Date #n#t#t*/ #tsTime.Hours = 0x1; #tsTime.Minutes = 0x0; #tsTime.Seconds = 0x0; #n #tif (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK) #t{ #t#t_Error_Handler(__FILE__, __LINE__); #t} #n #tDateToUpdate.WeekDay = RTC_WEEKDAY_MONDAY; #tDateToUpdate.Month = RTC_MONTH_JANUARY; #tDateToUpdate.Date = 0x1; #tDateToUpdate.Year = 0x0; #n #tif (HAL_RTC_SetDate(&hrtc, &DateToUpdate, RTC_FORMAT_BCD) != HAL_OK) #t{ #t#t_Error_Handler(__FILE__, __LINE__); #t} #n #t#tHAL_RTCEx_BKUPWrite(&hrtc,RTC_BKP_DR1,0x32F2); #t} #n} #n #n #nvoid HAL_RTC_MspInit(RTC_HandleTypeDef* rtcHandle) {#n #tif(rtcHandle->Instance==RTC) #t{ #t/* USER CODE BEGIN RTC_MspInit 0 */ #n#t/* USER CODE END RTC_MspInit 0 */ debuggg Expression usedDriverFlag is undefined on line 730, column 75 in ip_c.ftl. The problematic instruction: ---------- ==> ${usedDriverFlag} [on line 730, column 73 in ip_c.ftl] in user-directive generateServiceCode [on line 1234, column 5 in ip_c.ftl] ---------- Java backtrace for programmers: ---------- freemarker.core.InvalidReferenceException: Expression usedDriverFlag is undefined on line 730, column 75 in ip_c.ftl. at freemarker.core.TemplateObject.assertNonNull(TemplateObject.java:124) at freemarker.core.Expression.getStringValue(Expression.java:118) at freemarker.core.Expression.getStringValue(Expression.java:93) at freemarker.core.DollarVariable.accept(DollarVariable.java:76) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.MixedContent.accept(MixedContent.java:92) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.ConditionalBlock.accept(ConditionalBlock.java:79) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.MixedContent.accept(MixedContent.java:92) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.ConditionalBlock.accept(ConditionalBlock.java:79) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.IfBlock.accept(IfBlock.java:82) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.MixedContent.accept(MixedContent.java:92) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.ConditionalBlock.accept(ConditionalBlock.java:79) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.MixedContent.accept(MixedContent.java:92) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.IfBlock.accept(IfBlock.java:82) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.MixedContent.accept(MixedContent.java:92) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.Macro$Context.runMacro(Macro.java:164) at freemarker.core.Environment.visit(Environment.java:601) at freemarker.core.UnifiedCall.accept(UnifiedCall.java:106) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.MixedContent.accept(MixedContent.java:92) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.ConditionalBlock.accept(ConditionalBlock.java:79) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.MixedContent.accept(MixedContent.java:92) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.IfBlock.accept(IfBlock.java:82) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.MixedContent.accept(MixedContent.java:92) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.ConditionalBlock.accept(ConditionalBlock.java:79) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.MixedContent.accept(MixedContent.java:92) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.IteratorBlock$Context.runLoop(IteratorBlock.java:167) at freemarker.core.Environment.visit(Environment.java:415) at freemarker.core.IteratorBlock.accept(IteratorBlock.java:102) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.MixedContent.accept(MixedContent.java:92) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.Environment.visit(Environment.java:297) at freemarker.core.CompressedBlock.accept(CompressedBlock.java:73) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.ConditionalBlock.accept(ConditionalBlock.java:79) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.MixedContent.accept(MixedContent.java:92) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.ConditionalBlock.accept(ConditionalBlock.java:79) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.MixedContent.accept(MixedContent.java:92) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.IteratorBlock$Context.runLoop(IteratorBlock.java:167) at freemarker.core.Environment.visit(Environment.java:415) at freemarker.core.IteratorBlock.accept(IteratorBlock.java:102) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.MixedContent.accept(MixedContent.java:92) at freemarker.core.Environment.visit(Environment.java:208) at freemarker.core.Environment.process(Environment.java:188) at freemarker.template.Template.process(Template.java:237) at com.st.microxplorer.codegenerator.CodeEngine.freemarkerDo(CodeEngine.java:264) at com.st.microxplorer.codegenerator.CodeEngine.genCode(CodeEngine.java:185) at com.st.microxplorer.codegenerator.CodeGenerator.generateOutputCode(CodeGenerator.java:2553) at com.st.microxplorer.codegenerator.CodeGenerator.generatePeriphConfigCode(CodeGenerator.java:1483) at com.st.microxplorer.codegenerator.CodeGenerator.generateCodeFiles(CodeGenerator.java:1175) at com.st.microxplorer.codegenerator.CodeGenerator.generateCode(CodeGenerator.java:904) at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.generateCode(ProjectBuilder.java:1038) at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createCode(ProjectBuilder.java:931) at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:461) at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:41)2018-03-13 7:38 AM
Hello
Gwena.Munyaradzi
,This issue is fixed in the new CubeMx release.
So, please download and update the new
to fix this issue.Best Regards
Imen