Posted on February 23, 2018 at 00:55I am running version 4.24.0 of stm32cubeMX. I recently realized that when I try to generate any code the has rtc in it, the code generated in the rtc.c file is full of errors.I have tried on both Mac OSX and Win 7
Posted on February 26, 2018 at 13:32 DAHMEN.IMEN the Generated rtc.c file has this in it: /* Includes ------------------------------------------------------------------*/ #include 'rtc.h' #n #n /* USER CODE BEGIN 0 */ /* USER CODE END ...
Posted on February 26, 2018 at 13:31 Hi DAHMEN.IMEN Sorry I can't seem to be able to attach a file. I will have to send the the content of the ioc file. #MicroXplorer Configuration settings - do not modify FREERTOS.IPParameters=Tasks01 FRE...
Posted on February 26, 2018 at 12:57 , ,I'm using HAL the target IDE is System Workbench for STM32 , ♯ MicroXplorer Configuration settings - do not modify ,FREERTOS.IPParameters=Tasks01 ,FREERTOS.Tasks01=defaultTask,0,128,StartDefaultTask,Default,NU...