cancel
Showing results for 
Search instead for 
Did you mean: 

STM32W prevent execution of embedded serial boot loader

danielburgener9
Associate
Posted on March 27, 2013 at 11:58

If nBOOTMODE is asserted (pulled or driven low) when coming out of reset, the processor starts executing an embedded serial boot loader instead of its normal program. Is it possible to prevent this behaviour so that the embedded serial boot loader is no executed when the nBOOTMODE is low after a reset?

2 REPLIES 2
tlamotte9
Associate II
Posted on September 15, 2014 at 17:33

Dear all,

I am just looking for the same anwser to dandu's question because I need to prevent entry to the System memory boot loader even if BOOT0 is driven low.

Do any Option Bytes help for that?

Is anybody from ST could reply?

Best regards,

Thierry

Posted on September 15, 2014 at 18:25

Probably not, and perhaps something you'd discuss with your FAE, or local rep.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..