2019-11-13 02:19 PM
The STM32VL-DISCOVERY is seen by the computer as a disc and not as a serial port.
I use win7. How to solve the problem?
2019-11-13 05:32 PM
Look in the device manager, if there's some USB device with driver not installed. This is the serial port. Download and install the driver for it.
2019-11-13 10:15 PM
> The STM32VL-DISCOVERY is seen by the computer as a disc and not as a serial port.
This is the way the V1 version of the ST-Link was implemented.
Probably by an intern, because ST did cover itself with glory in this case.
Check if your toolchain supports this old version, or better, get a better board.
2019-11-13 11:11 PM
I don't have a usb device without a driver
2019-11-13 11:13 PM
Another detail is that the board is correctly programmed.