cancel
Showing results for 
Search instead for 
Did you mean: 

STM32VL-DISCOVERY

TFerg.1136
Associate II

The STM32VL-DISCOVERY is seen by the computer as a disc and not as a serial port.

I use win7. How to solve the problem?

0690X00000As0loQAB.jpg

4 REPLIES 4
Pavel A.
Evangelist III

Look in the device manager, if there's some USB device with driver not installed. This is the serial port. Download and install the driver for it.

Ozone
Lead III

> The STM32VL-DISCOVERY is seen by the computer as a disc and not as a serial port.

This is the way the V1 version of the ST-Link was implemented.

Probably by an intern, because ST did cover itself with glory in this case.

Check if your toolchain supports this old version, or better, get a better board.

I don't have a usb device without a driver

TFerg.1136
Associate II

Another detail is that the board is correctly programmed.