2024-01-03 9:54 PM
I am confused:
I have a PCB designed for STMU575 and I am using USB FS - works.
USB DM and DP are pins PA11 and PA12.
On U575:
- all fine as USB FS, available via AF10 (PA11 = OTG_FS_DM, OTG_FS_DM) - works
I have checked the packages and pin assignments and saw: U5A5 is identical with U5A5 (and I want to solder U5A5 due to larger memories instead of U575).
But UA5A datasheet is a bit different on PA11, PA12:
1. it mentions "OTG_HS_DM(boot)" as "additional functions"
2. in pin mux ALT table: there is nothing under ALT10 - there is NOT an ALT option to configure PA11, PA12 as USB pin
My questions:
a) changing from U575 to a U5A5 on same PCB and package (LQPF64) - are PA11 and PA12 usable in the same way as USB (FS)?
b) if changing to U5A5 and PA11, PA12 become OTG_HS_DM, OTH_HS_DP now: does it mean I have to configure now USB HS instead of USB FS (as on U575)?
c) how to configure ALT function of USB_HS (if not listed in table) for U5A5?
Solved! Go to Solution.
2024-07-11 10:20 AM
My project is here:
https://github.com/tjaekel/NUCLEO-U5A5JZ-Q_QSPI
I think, important is:
ATT: I saw, that not all possible combinations of PLL config is working, e.g. PLLM seems to be as "must be 1".
//8 MHz OSC, my board
RCC_OscInitStruct.PLL.PLLM = 1; //2; ==> THIS FAILS on USB
RCC_OscInitStruct.PLL.PLLN = 40; //20; ==> THIS FAILS on USB
RCC_OscInitStruct.PLL.PLLP = 10; //32 MHz, USB with PLL2_P_DIV2! (as 16 MHz)
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2; //should result in 160 MCU clock
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_1;
PeriphClkInit.UsbPhyClockSelection = RCC_USBPHYCLKSOURCE_PLL1_DIV2;
So, with your 32 MHz HSE, try this PLL config:
//with 32MHz HSE:
.PLL.PLLM = 1,
.PLL.PLLN = 10,
.PLL.PLLP = 10, //32MHz for USB, use RCC_USBPHYCLKSOURCE_PLL1_DIV2
.PLL.PLLQ = 2,
.PLL.PLLR = 2,
.PLL.PLLRGE = RCC_PLLVCIRANGE_1,
.PLL.PLLFRACN = 0,