2025-02-04 12:40 PM
Hello Everyone!
I am facing an issue while trying to enter the STM32 bootloader via USART1 on an STM32U599ZJT.
When applying 3.3V to BOOT0 and performing a single reset, the MCU enters a reset (boot?) loop, which persists until BOOT0 is deasserted.
However, when BOOT0 → GND, the reset loop stops, and the MCU behaves normally.
Any insights on what might be causing this behavior would be greatly appreciated!
Thank you in advance for your help!
Solved! Go to Solution.
2025-02-13 11:49 AM
The USB_DM pin (PA12) must be pulled high with a strong pull-up resistor (maximum 2.7kΩ).
2025-02-13 11:49 AM
The USB_DM pin (PA12) must be pulled high with a strong pull-up resistor (maximum 2.7kΩ).