STM32U585 + SAI
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-01-26 1:14 AM
Dear Sir.
I use ICS-43434 connected to STM32U585 through SAI.
The lines of the ICS-43434 SD,SCK,WS works fine ,
But when the interrupt is enabled the program crash.
Attached some code frgaments.
Main.c.
MX_SAI1_Init();
static void MX_SAI1_Init(void)
{
/* USER CODE BEGIN SAI1_Init 0 */
/* USER CODE END SAI1_Init 0 */
/* USER CODE BEGIN SAI1_Init 1 */
/* USER CODE END SAI1_Init 1 */
hsai_BlockA1.Instance = SAI1_Block_A;
hsai_BlockA1.Init.AudioMode = SAI_MODEMASTER_RX;
hsai_BlockA1.Init.Synchro = SAI_ASYNCHRONOUS;
hsai_BlockA1.Init.OutputDrive = SAI_OUTPUTDRIVE_ENABLE; //SAI_OUTPUTDRIVE_ENABLE;//SAI_OUTPUTDRIVE_DISABLE;
hsai_BlockA1.Init.NoDivider = SAI_MASTERDIVIDER_ENABLE;//SAI_MASTERDIVIDER_DISABLE;//SAI_MASTERDIVIDER_ENABLE;
hsai_BlockA1.Init.FIFOThreshold = SAI_FIFOTHRESHOLD_EMPTY;//SAI_FIFOTHRESHOLD_FULL;//SAI_FIFOTHRESHOLD_EMPTY;
hsai_BlockA1.Init.AudioFrequency = SAI_AUDIO_FREQUENCY_16K;
hsai_BlockA1.Init.SynchroExt = SAI_SYNCEXT_DISABLE;
hsai_BlockA1.Init.MckOutput = SAI_MCK_OUTPUT_DISABLE;
hsai_BlockA1.Init.MonoStereoMode = SAI_MONOMODE;
hsai_BlockA1.Init.CompandingMode = SAI_NOCOMPANDING;
hsai_BlockA1.Init.TriState = SAI_OUTPUT_NOTRELEASED;//SAI_OUTPUT_RELEASED ; //SAI_OUTPUT_NOTRELEASED;
if (HAL_SAI_InitProtocol(&hsai_BlockA1, SAI_I2S_STANDARD, SAI_PROTOCOL_DATASIZE_24BIT,2) != HAL_OK)
// if (HAL_SAI_InitProtocol(&hsai_BlockA1, SAI_I2S_MSBJUSTIFIED, SAI_PROTOCOL_DATASIZE_24BIT,2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SAI1_Init 2 */
/* USER CODE END SAI1_Init 2 */
}
audio_len = 4096;
AL_SAI_Receive_IT(&hsai_BlockA1, &audio[0],audio_len);
HAL_StatusTypeDef HAL_SAI_Receive_IT(SAI_HandleTypeDef *hsai, uint8_t *pData, uint16_t Size)
{
if ((pData == NULL) || (Size == 0U))
{
return HAL_ERROR;
}
if (hsai->State == HAL_SAI_STATE_READY)
{
/* Process Locked */
__HAL_LOCK(hsai);
hsai->pBuffPtr = pData;
hsai->XferSize = Size;
hsai->XferCount = Size;
hsai->ErrorCode = HAL_SAI_ERROR_NONE;
hsai->State = HAL_SAI_STATE_BUSY_RX;
if ((hsai->Init.DataSize == SAI_DATASIZE_8) && (hsai->Init.CompandingMode == SAI_NOCOMPANDING))
{
hsai->InterruptServiceRoutine = SAI_Receive_IT8Bit;
}
else if (hsai->Init.DataSize <= SAI_DATASIZE_16)
{
hsai->InterruptServiceRoutine = SAI_Receive_IT16Bit;
}
else
{
hsai->InterruptServiceRoutine = SAI_Receive_IT32Bit;
}
/* Enable TXE and OVRUDR interrupts */
__HAL_SAI_ENABLE_IT(hsai, SAI_InterruptFlag(hsai, SAI_MODE_IT));
/* Check if the SAI is already enabled */
if ((hsai->Instance->CR1 & SAI_xCR1_SAIEN) == 0U)
{
/* Enable SAI peripheral */
__HAL_SAI_ENABLE(hsai);
}
/* Process Unlocked */
__HAL_UNLOCK(hsai);
return HAL_OK;
}
else
{
return HAL_BUSY;
}
}
stm32u5xx_hal_msp.c
static uint32_t SAI1_client =0;
void HAL_SAI_MspInit(SAI_HandleTypeDef* hsai)
{
GPIO_InitTypeDef GPIO_InitStruct;
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
/* SAI1 */
if(hsai->Instance==SAI1_Block_A)
{
/* Peripheral clock enable */
/** Initializes the peripherals clock
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_SAI1;
PeriphClkInit.Sai1ClockSelection = RCC_SAI1CLKSOURCE_PLL2;
PeriphClkInit.PLL2.PLL2Source = RCC_PLLSOURCE_MSI;
PeriphClkInit.PLL2.PLL2M = 3;//4; //3;
PeriphClkInit.PLL2.PLL2N = 8;//20;//8;
PeriphClkInit.PLL2.PLL2P = 1;//5;//1;
PeriphClkInit.PLL2.PLL2Q = 2;
PeriphClkInit.PLL2.PLL2R = 2;
PeriphClkInit.PLL2.PLL2RGE = RCC_PLLVCIRANGE_1;
PeriphClkInit.PLL2.PLL2FRACN = 0.0;
PeriphClkInit.PLL2.PLL2ClockOut = RCC_PLL2_DIVP;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
if (SAI1_client == 0)
{
__HAL_RCC_SAI1_CLK_ENABLE();
/* Peripheral interrupt init*/
HAL_NVIC_SetPriority(SAI1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(SAI1_IRQn);
}
SAI1_client ++;
/**SAI1_A_Block_A GPIO Configuration
PE5 ------> SAI1_SCK_A
PE4 ------> SAI1_FS_A
PE6 ------> SAI1_SD_A
*/
GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_4|GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF13_SAI1;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
}
}
stm32u5xx_it.c
SAI_HandleTypeDef hsai_BlockA1;
void SAI1_IRQHandler(void)
{
// static uint8_t a = 0;
//
// switch(a)
// {
// case 0 : HAL_GPIO_WritePin(GPIOD, GPIO_PIN_0, GPIO_PIN_RESET);
// a = 1;
// break;
// case 1 : HAL_GPIO_WritePin(GPIOD, GPIO_PIN_0, GPIO_PIN_SET);
// a = 0;
// break;
// }
/* USER CODE BEGIN SAI1_IRQn 0 */
/* USER CODE END SAI1_IRQn 0 */
HAL_SAI_IRQHandler(&hsai_BlockA1);
/* USER CODE BEGIN SAI1_IRQn 1 */
/* USER CODE END SAI1_IRQn 1 */
}
even if I comment out the line HAL_SAI_IRQHandler(&hsai_BlockA1);
still the program crashes
Please Advise.
- Labels:
-
SAI
-
STM32U5 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-02-16 12:53 AM
Hello @Community member and welcome to the community,
What kind of error/crash you have?, is it hardfault?
Mohamed Aymen