cancel
Showing results for 
Search instead for 
Did you mean: 

USBX driver CDC virtual comport

SKCL-1
Associate II

Hi,

While configuring STM32U585 controller USBX driver CDC virtual comport device is not showing in device manager. Pl provide sample code for STM32U585VIT6. This is out custom board with a USB port acting as device to the PC.

2 REPLIES 2
FBL
ST Employee

Hi @SKCL-1 

If you can share the USB schematics, your firmware configuration and additional details it will be easier to help you further investigate the issue.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
SKCL-1
Associate II

SKCL1_0-1744184023788.png

SKCL1_1-1744184046302.png

Attached schematic of the USB section. 

SKCL1_2-1744184077277.png

We are looking for firmware support, so that we can see virtual com board. THe board is working so clk and other areas are no issues, Currently we are drawing power from the 2-usb ports