cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U575 Legacy USBD MSC without Azure USBX Tutorial

DK3
Associate II

Hi,

I want to implement USBD MSC using lagecy middle ware and use an SD card as storage.

Is there a tutorial like this ? 

STM32U585 Legacy CDC without Azure USBX Tutorial - STMicroelectronics Community

Best regards.

1 REPLY 1
FBL
ST Employee

Hi @DK3 

You can follow the examples provided to use classic library then configure the USB device middleware MSC class.

If you encounter issues during the implementation, you can refer to the resources and ask directly specific questions. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.