2022-02-28 04:40 AM
Hello
I use a STM32U575 develop board to do the ADC sampling. The inject signal is 10mV RMS with 1.648V bias voltage
However, from the sampling result, there is a obviously break point in the result.
Could you help explain the reason and how to eliminate the error
2022-03-06 05:06 AM
Who can support on this topic?
Thanks!
2022-03-07 09:08 PM
Well first check the errata sheet, then calibrate the adc if not done, then the sw that output the adc converted values is bug free.