2023-08-10 09:35 AM
Hello. We are building a widget using the new STM32U5 (BGA) device. So far, so good. Need to have an onboard STLINK 2.1 with drag & drop feature to allow for easy to use end user firmware upgrades. Could someone please confirm that the STLINK v2.1 is supporting of the STM32U5 targets? The latest STLINK hardware is just too pricey to including on a consumer design. Thanks in advance.
2023-08-10 11:00 AM