2025-04-04 2:58 AM
Good day,
I'm experiencing an unexplained bus fault when the MCU writes to unaligned (not aligned to 32-bit) addresses in the OSPI memory region. I've written a minimal implementation that shows where the issue occurs. See below.
I'm using the STM32U585 with two IS66WVS4M8BLL quad SPI modules. The OctoSPI peripheral is configured in Dual-Quad Mode. See the image for the settings as configured in STM32CubeMX. I use memory mapped mode. I've enabled DQS for writes as per 2.6.1 of the errata. I've tried different MPU cache configurations for this area: no MPU, MPU_DEVICE_nGnRnE, and (MPU_WRITE_THROUGH | MPU_NON_TRANSIENT | MPU_W_ALLOCATE | MPU_R_ALLOCATE).
Here's the minimal implementation. Note that 8-bit writes work if the previous write was aligned. See comments surrounded by ***, focussing on Test 2.
// Test 1: Unaligned 8-bit access
// *** This first test works without issues ***
volatile uint32_t sramByteLoopIndex;
volatile __IO uint8_t *mem_addr_byte;
volatile uint8_t sramTestValByte;
// Writing Sequence (8-bit, unaligned pattern)
mem_addr_byte = (uint8_t *)(OCTOSPI1_BASE);
for (sramByteLoopIndex = 0; sramByteLoopIndex < OSPI_MEM_SIZE_BYTES;
sramByteLoopIndex++)
{
sramTestValByte = (uint8_t)(sramByteLoopIndex &
0xFF); // Use lower 8 bits of index as pattern
*mem_addr_byte = sramTestValByte;
mem_addr_byte += 1;
}
// Reading Sequence (8-bit, unaligned check)
mem_addr_byte = (uint8_t *)(OCTOSPI1_BASE);
for (sramByteLoopIndex = 0; sramByteLoopIndex < OSPI_MEM_SIZE_BYTES;
sramByteLoopIndex++)
{
sramTestValByte = (uint8_t)(sramByteLoopIndex & 0xFF);
assert_param(*mem_addr_byte == sramTestValByte);
mem_addr_byte += 1;
}
// Test 2: Unaligned Copy within SRAM
// *** Here things are not well ***
volatile __IO uint8_t *src_addr_byte;
volatile __IO uint8_t *dst_addr_byte;
volatile uint8_t test_pattern_byte;
const uint32_t copy_size_bytes = 512; // Size of data to copy
// Ensure source and destination are unaligned and distinct
const uint32_t src_offset = 1; // Unaligned source start
const uint32_t dst_offset =
(OSPI_MEM_SIZE_BYTES / 2) + 3; // Unaligned destination start
// Ensure offsets are valid and don't cause wrap-around issues with copy size
if ((src_offset + copy_size_bytes < OSPI_MEM_SIZE_BYTES) &&
(dst_offset + copy_size_bytes < OSPI_MEM_SIZE_BYTES))
{
// Dummy aligned write first
// *** Removing this line causes BusFault on the write in code block 1 below ***
*((volatile __IO uint8_t *)OCTOSPI1_BASE) = 0;
// 1. Fill source region with a pattern
src_addr_byte = (uint8_t *)(OCTOSPI1_BASE + src_offset);
for (sramByteLoopIndex = 0; sramByteLoopIndex < copy_size_bytes;
sramByteLoopIndex++)
{
test_pattern_byte =
(uint8_t)((sramByteLoopIndex + 0xAA) & 0xFF); // Arbitrary pattern
*src_addr_byte = test_pattern_byte; // *** BusFault here on first iteration if the dummy write is commented out, otherwise no issues here ***
src_addr_byte++;
}
// 2. Perform byte-by-byte unaligned copy (Isolated Read/Write)
src_addr_byte = (uint8_t *)(OCTOSPI1_BASE + src_offset);
dst_addr_byte = (uint8_t *)(OCTOSPI1_BASE + dst_offset);
volatile uint8_t temp_byte; // Temporary variable
for (sramByteLoopIndex = 0; sramByteLoopIndex < copy_size_bytes;
sramByteLoopIndex++)
{
temp_byte = *src_addr_byte;
__asm__ __volatile__ ("nop"); // Tried adding NOP as per 2.6.10 of errata, even though we are not using DTR
*dst_addr_byte = temp_byte; // *** BusFault here on first iteration if the dummy aligned write is preset***
src_addr_byte++;
dst_addr_byte++;
}
// 3. Verify destination region
// *** We never get here ***
dst_addr_byte = (uint8_t *)(OCTOSPI1_BASE + dst_offset);
for (sramByteLoopIndex = 0; sramByteLoopIndex < copy_size_bytes;
sramByteLoopIndex++)
{
test_pattern_byte =
(uint8_t)((sramByteLoopIndex + 0xAA) & 0xFF); // Expected pattern
assert_param(*dst_addr_byte == test_pattern_byte);
dst_addr_byte++;
}
}I can post my memory mapped initialisation code, if needed.
Any suggestions of what I might be missing, or how to move forward?
@Alex - APMemory have you ever seen something like this?
Solved! Go to Solution.
2025-04-10 12:55 AM - edited 2025-04-10 12:56 AM
Just to close the loop on this:
I disabled all caching options (MPU, DCACHE, ICACHE) and the problem still occured at the same location. The OSPI peripheral does have an internal FIFO, perhaps that is playing a role here. The documentation mentions that it is involved in in read operations. Perhaps there is undocumented use of the FIFO for write operations?
Regardless, it seems that even addresses (and even number of bytes) is a requirement for my configuration of dual memory and that is the answer to my original question.