cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6 Debug Jump From FSBL to Secure Application

aroby95
Associate

Currently, I have a project using a secure application for the STM32N6570-DK. I am able to run and debug the FSBL and Application with the system in Dev Boot, but have yet to be able to attach and debug when booting from the external flash (Boot1 and Boot0 both LOW).

I have placed the following code toward the beginning of my FSBL, and configured my  STM32CubeIDE debug to not load the program, and the not reset the chip when attaching for debug. However, I am still unable to attach and debug the system.

__HAL_RCC_BSEC_CLK_ENABLE(); BSEC->AP_UNLOCK = 0xB4; BSEC->DBGCR = 0xB4B4B400; __asm("bkpt 255");

 Has anyone been able to debug their application with the MCU booting from external flash?

4 REPLIES 4
Amel NASRI
ST Employee

Hi @aroby95 ,

Probably you find some help in the article How to create an STM32N6 FSBL load and run (focus on second application case).

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Joe WILLIAMS
ST Employee

Hi aroby95

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards

Joe

STMicro Support

Hello @aroby95  @Joe WILLIAMS ,

I’m experiencing the same issue. I wonder what the solution is?

Best regards,

Egemen Aksoy

ERROR
Associate III

Hi,

I use the following approach for the XIP configuration.

The FSBL is without changes.

In the Appli code, in main.c, add code as shown below. Make sure that the debugger does load symbols from Aplpli ELF only, and does not download the firmware, and does not reset the chip (see the pics below).

Now you can power up (or reset) the board after flashing, run the Appli debug, set breakpoints and press the USER1 button to debug.

BSP_PB_Init (BUTTON_USER1, BUTTON_MODE_GPIO); // loop that can be used to catch the application for debug.Set mini to 1, build and flash target as normally. // Set BOOT1 switch to the left position, press reset without removing cable. // Use the Connect to running debug config to connect, then change mini value from watch. // For breakpoints to work they seem to need to be manually changed to ahrdware breakpoint static volatile int debugFlag = 1; while (debugFlag == 1 && BSP_PB_GetState(BUTTON_USER1) == 0) { __NOP(); } /* USER CODE END 1 */

 

ERROR_0-1749360279856.png

ERROR_1-1749360331215.png