cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L4xx reference manuals System clock (SYSCLK) selection

berendi
Principal

RM0351 and RM0392 (and maybe others, haven't checked them all) contain this in the System clock (SYSCLK) selection section

Status bits in the Internal clock sources calibration register (RCC_ICSCR) indicate which clock(s) is (are) ready and which clock is currently used as a system clock.

However the various clock ready and system clock switch status bits are actually located in RCC->CR and RCC->CFGR.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee

Hello,

I raised this internally for update.

Thank you for your contribution.

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
waclawek.jan
Super User

Hi @Imen DAHMEN​ ,

I've seen the same sentence also in RM0440 and RM0444, so this propagates across families.

Jan