cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L4S9 SAI Configuration Full Duplex

NKara.3
Associate II

Hi,

I would like to use the SAI as full duplex slave mode with I2S/PCM protocol.

I'm not sure about the configuration and which pins are TX and RX when using Cube.

0693W00000DqI2kQAF.png 

In the parameter I can set the audio to transmit or receive.

In this case SAI_SD_A will be transmit and SAI_SD_B receive?

0693W00000DqI5AQAV.png

1 REPLY 1
Bruno_ST
ST Employee

Hello @NKara.3​ 

Yes, your setup looks correct to me.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.