cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L4A6 Exiting Stop Mode 1 using UART

jlsw30
Associate II

Hi, 

Using references from 

1) STML496 UART Wake up from Stop Example - https://github.com/STMicroelectronics/STM32CubeL4/blob/master/Projects/NUCLEO-L496ZG/Examples/UART/UART_WakeUpFromStop/Src/main.c#L78 

2) STM Getting started with PWR Guide - https://wiki.st.com/stm32mcu/wiki/Getting_started_with_PWR#Stop0.2C_Stop1.2C_and_Stop2_modes

I have the following code that tries to wake up from STOP1 via UART. 

 

/* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_I2C1_Init(); MX_UART5_Init(); /* USER CODE BEGIN 2 */ HAL_PWREx_EnableLowPowerRunMode(); /* USER CODE END 2 */ __HAL_RCC_WAKEUPSTOP_CLK_CONFIG(RCC_STOP_WAKEUPCLOCK_MSI); /* make sure that no UART transfer is on-going */ while(__HAL_UART_GET_FLAG(&huart5, UART_FLAG_BUSY) == SET); /* make sure that UART is ready to receive * (test carried out again later in HAL_UARTEx_StopModeWakeUpSourceConfig) */ while(__HAL_UART_GET_FLAG(&huart5, UART_FLAG_REACK) == RESET); WakeUpSelection.WakeUpEvent = UART_WAKEUP_ON_READDATA_NONEMPTY; if (HAL_UARTEx_StopModeWakeUpSourceConfig(&huart5, WakeUpSelection)!= HAL_OK) { Error_Handler(); } /* Enable the UART Wake UP from STOP1 mode Interrupt */ __HAL_UART_ENABLE_IT(&huart5, UART_IT_WUF); /* enable MCU wake-up by UART */ HAL_UARTEx_EnableStopMode(&huart5); /* enter STOP1 mode */ DEBUG_Transmit((uint8_t *)"Entering stop mode\r\n", 20); HAL_SuspendTick(); HAL_PWREx_EnterSTOP1Mode(PWR_SLEEPENTRY_WFI); HAL_ResumeTick(); DEBUG_Transmit((uint8_t *)"success\r\n", 9); /* at that point, MCU has been awoken: the LED has been turned back on */ SystemClock_Config(); /* Wake Up based on RXNE flag successful */ HAL_UARTEx_DisableStopMode(&huart5);
View more

 

 However, the interrupt does not seem to trigger and i am always stuck in stop mode.

I have also attached my clock configuration as follows.

jlsw30_0-1726736464496.png

Appreciate any advise on what I am doing wrong. Thank you. 

1 ACCEPTED SOLUTION

Accepted Solutions
jlsw30
Associate II

Solved this by adjusting clock to not use MSI, though this is not an optimal solution as i would prefer a lower clock speed configuration for my usage. Will try to see how i can modify the code to work with MSI clock configuration. 

View solution in original post

4 REPLIES 4
Sarra.S
ST Employee

Hello @jlsw30, welcome to ST Community, 

To be sure that the UART is not busy with any ongoing transmission or reception and the UART receiver is enabled and ready to receive data: 

while(__HAL_UART_GET_FLAG(&UartHandle, USART_ISR_BUSY) == SET); /* make sure that UART is ready to receive * (test carried out again later in HAL_UARTEx_StopModeWakeUpSourceConfig) */ while(__HAL_UART_GET_FLAG(&UartHandle, USART_ISR_REACK) == RESET)

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello Sarra, thank you for the reply. 

Initially thought I had to use a different flag as it was UART5 instead of USART5 on STML4A6. 

Either way, I have tried the code as recommmended but was still unable to wake up from stop mode.  

while(__HAL_UART_GET_FLAG(&UartHandle, USART_ISR_BUSY) == SET); /* make sure that UART is ready to receive * (test carried out again later in HAL_UARTEx_StopModeWakeUpSourceConfig) */ while(__HAL_UART_GET_FLAG(&UartHandle, USART_ISR_REACK) == RESET)

In the datasheet, UART 5 is able to wake stop1, so i believe that it should be possible 

jlsw30_0-1726797071203.png

I have also attached my callbacks as follows for reference:

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) { if (huart->Instance == UART5) { HAL_ResumeTick(); /* at that point, MCU has been awoken: the LED has been turned back on */ SystemClock_Config(); /* Handle received data */ DEBUG_Transmit((uint8_t *)"Data received\r\n", 15); } } void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart) { if (huart->Instance == UART5) { DEBUG_Transmit((uint8_t *)"Data transmitted\r\n", 18); } } void HAL_UART_ErrorCallback(UART_HandleTypeDef *huart) { if (huart->Instance == UART5) { DEBUG_Transmit((uint8_t *)"UART Error\r\n", 12); } }

Thank you!

jlsw30
Associate II

I have attached my .ioc file and main.c file for reference

jlsw30
Associate II

Solved this by adjusting clock to not use MSI, though this is not an optimal solution as i would prefer a lower clock speed configuration for my usage. Will try to see how i can modify the code to work with MSI clock configuration.