cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L432KC: which reference manual should I use ?

Kraal
Senior III
Posted on May 19, 2017 at 08:30

Hello everyone,

Can somebody please explain me what are the differences between RM0393 (which is specific to STM32L4x2, but latest release is from May 2016) and RM0394 (which is specific to STM32L43xxx and so on and latest release is from April 2017) ? If I want to use the STM32L432KC device, which one should I use ?

Thanks.

#reference-manual #stm32l4 #stm32l432
2 REPLIES 2
Imen.D
ST Employee
Posted on May 26, 2017 at 17:19

Hi

Kjeldsen.Carl_Nicola

,

You can use the last reference manual RM0394 (

latest release

published in April 2017)

In fact,STM32L432 andSTM32L442 were covered by RM0393, but now we are going to update the reference manual RM0394to support and integrate STM32L43xxx/

STM32L

44xxx.

Then the old reference RM0393 will become hidden from the website.

Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on May 27, 2017 at 11:51

Hi

DAHMEN.IMEN

,

Many thanks for the info.

Have a nice day,

Kraal