2018-06-21 11:35 AM
Hi,
With the cubeMx tool, when i use usart2 , the lpuart can not be included.
But when i set as bellow, is it possible to use usart2 tx/rx full duplex, and lpuart tx only ?
-- as follows--
Usart2
TX : PA2
RX: PA15
LPUART
TX : PA3
RX :
(!! with pin swap option)
Thanks in advance.
2018-06-21 11:45 AM
The GPIO and AF settings should be able to achieve that.