cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L412 | How to fix MCU getting hung up in HAL peripheral init functions

GBrac.3
Associate II

While in debug mode if I step through the HAL init functions (the first one I have trouble with is COMP1_Init()) I get stuck in a loop that does nothing but decrement a counter. There is no timer associated with the loop it just looks like a while(timeout) { timeout--;}. I have a breakpoint before and after so I know that the loop is where I get stuck. If I hit run at the beginning of the program I get to the breakpoint before the loop, but when I hit run again I never reach the post-loop breakpoint. Any suggestions would be appreciated. I found a couple of forum posts with a similar issue but they were all fixed by cycling power. I have tried cycling power, restarting my IDE, restarting my debugger, with no luck.

Thanks in advance for the help!

EDIT 1:

After doing more debugging it seems that there are a few more problems, any time something calls the HAL_Delay() function it also hangs up but if I manually step through the function it is fine, maybe there is something in the debug configuration that could affect this but I haven't found it yet. I have a similar problem when starting TIM1. I am able to initialize it with no issues but when I call HAL_TIM_Base_Start_IT() it gets hung up if I try to step over it but if I step into it then it works just fine.

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Bob S
Principal

Some interrupt firing and never returning, or continually firing and starving the main code of CPU cycles? If you halt execution, where is the CPU? This is in HAL_COMP_Init() waiting for the scaler bridge voltage to stabilize, right? Can you step into the while() loop and see the value decrement?

GBrac.3
Associate II

It could definitely be some interrupt firing and never returning, but when I halt execution I get error saying that the debugger doesn't know where I am in the code, thus I haven't been able to see what is doing the interrupting. It is waiting for the bridge voltage to stabilize, I can step through the while loop and it seems to go fine for at least the first few cycles but I don't want to sit at my computer hitting F6 5000 times to get through the loop.

GBrac.3
Associate II

And another quick edit, while I wasn't able to see where the code it was getting stuck I was still able to step the disassembly and it kept going back to a loop that started either at address 0x1fff_2171 or 0x1fff_225a, it's a little hard to tell because I'm just clicking through assembly code.

How is BOOT0 pin connected? How are the Option bytes set?

JW

GBrac.3
Associate II

The BOOT0 Pin was left floating on this version of the PCB, so I have nSWBOOT0 = 0 so that boot configuration is handled by the option bytes. nBOOT0 = 0 and nBOOT1 = 1 to when programming. I have also tried nSWBOOT0 = 1, nBOOT0 = 0, and nBOOT1 = 1 and was able to flash the program but any other combinations have been unable to flash the memory