2017-05-03 06:39 AM
Hi,
We have a custom designed STM32L151R board. We have not been able to flash the code using the flash loader application (demonstrator gui) . We are able to load the code using ST-Link and the serial port works properly when configured through the code. Is this an inherent problem of the controller or are we doing something wrong? We need to get the serial boot loader working as there may be site updates. Thank you for your time. Awaiting your suggestions to solve the problem.
Note: this post was migrated and contained many threaded conversations, some content may be missing.2017-05-03 08:50 AM
>>
Is this an inherent problem of the controller or are we doing something wrong?
Most likely the latter. Not familiar with your design.
2017-05-04 08:36 AM
Hi
Nayani.Parmin
,Please precise the device part numberyou are using.
2017-05-04 09:46 PM
Hi CliveOne,
The design is pretty simple. USART1 Rx, Tx pins are level shifted (RS232) and brought out on to a connector along with GND. These pins are used only for UART and nothing else. We have jumpers on BOOT pins. USB is not being used. Controller is going in to boot mode but is not responding to boot loader. Remaining pins are used as I/Os, SPI etc. Hope this clarifies. Thanks.
2017-05-04 10:19 PM
Hi Imen D,
The exact part number is STM32L151RBT6A. Hope this helps. Thank you.
2017-05-07 11:59 PM
Hello,
Look at
and make sure for the details regarding your device.Make sure there is no activity on the other bootloader pins because the bootloader may select another communication interface.
2017-05-08 02:29 AM
The design is pretty simple. USART1 Rx, Tx pins are level shifted (RS232) and brought out on to a connector along with GND
Have you checked the signals at RX during boot ?
Level shifters might be inverting, or not.
2017-05-08 03:13 AM
Hi AvaTar,
Yes I have checked the level shifter and it works fine. As mentioned in my first post, once code is flashed into the controller using ST Link, the serial port works fine (both receive and transmit). The issue is when the controller is in boot mode. It just does not respond. Thank you.
Regards
2017-05-08 03:17 AM
Hi Max,
Thanks for the advice. It is precisely for this reason that I mentioned that USB is not being used (USB for flashing). I have also put a pull-up resistor on USART2 Rx pin so no untoward signals appear on the pin and push controller into looking at that pin for boot commands. However I will go through the reference you mentioned and revert.
Best wishes.
2017-05-08 08:58 AM
Well you're going to need to go back to first principles, bring the chip up in the System Loader and talking to it via something like RealTerm at 9600 8E1, use hex mode and send the 0x7F symbol, see if the device responds with the 0x79, and if it does walk through a couple of the documented commands the loader should recognize. Start with the identification and versioning commands.
If it doesn't work at this level the application isn't going to work either. Use a logic analyzer to record the device reset and USART1_TX/RX pin transactions through the dispatch of the 0x7F and the response.