cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L053DISCO - How to enable 3V_O or 5V_O

Thomas L.
Associate III

In the document UM1775 there is stated the following:

"5 V and 3 V can be used as output power supplies when an extension board is

connected to pins P2 and P3.

...

In this case, the 5V_O and 3V_O pins deliver a 5 V or 3.3 V power supply and the

power consumption of the extension board must be lower than 100 mA."

Yet, the Supply for 3V_O is gated through T2 which in turn is controlled by PB15 on the SM32F103 (PWR_ENn); I guess that this is the controller which handles the ST-Link and cannot be changed.

How does this controller determine if there is an extension board connected to P2 or P3 so that it enables that supply?

1 ACCEPTED SOLUTION

Accepted Solutions

PWR_ENn enables power to the whole board, including the target, when the STLink sucessfully enumerates (or if this is overriden using the JP2 jumper).

Note, that 3V_OUT is shorted to 3V3.

JW

View solution in original post

2 REPLIES 2

PWR_ENn enables power to the whole board, including the target, when the STLink sucessfully enumerates (or if this is overriden using the JP2 jumper).

Note, that 3V_OUT is shorted to 3V3.

JW

Thomas L.
Associate III

Oh I see. Thanks, that makes sense