cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L031K6 ISP not work

xle.1
Associate II

STM32 only connect VCC and UART2. Can it download programs with ISP(UART2 PA2-3)?

1 ACCEPTED SOLUTION

Accepted Solutions

Thanks I've solved it​

Chip failure

View solution in original post

4 REPLIES 4

> Can it download programs with ISP(UART2 PA2-3)?

For individual bootloader options, check AN2606.

Isn't there activity on other bootloader interfaces' pins? If yes, the bootloader may errorneously think that communication goes there.

BOOT0 is connected how? NRST is connected how?

Communication is provided how? Check using oscilloscope the waveform on the UART_Rx pin.

Does the chip work at all? Check all VDD/GND pins. Is power supply OK?

It's always better to start with a "known good" hardware e.g. a Nucleo board, which has also USB-VCP support in its on-board STLink.

JW

Show a schematic.

If analogue supply pins, make sure they are wired too.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks I've solved it​

Chip failure

Thanks I've solved it​

Chip failure