cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L011K4T6 SPI CLK Problems

RSchu.1
Associate II
/* USER CODE BEGIN Header */
/**
  ******************************************************************************
  * @file           : main.c
  * @brief          : Main program body
  ******************************************************************************
  * @attention
  *
  * <h2><center>&copy; Copyright (c) 2020 STMicroelectronics.
  * All rights reserved.</center></h2>
  *
  * This software component is licensed by ST under BSD 3-Clause license,
  * the "License"; You may not use this file except in compliance with the
  * License. You may obtain a copy of the License at:
  *                        opensource.org/licenses/BSD-3-Clause
  *
  ******************************************************************************
  */
/* USER CODE END Header */
 
/* Includes ------------------------------------------------------------------*/
#include "main.h"
 
 
SPI_HandleTypeDef hspi1;
 
 
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_SPI1_Init(void);
/* USER CODE BEGIN PFP */
 
 
int main(void)
{
 
  HAL_Init();
 
 
  SystemClock_Config();
 
 
  MX_GPIO_Init();
  MX_SPI1_Init();
 
    RCC->IOPENR |=RCC_IOPENR_GPIOAEN;
    RCC->IOPENR |=RCC_IOPENR_GPIOBEN;
    RCC->APB2ENR|= RCC_APB2ENR_SPI1EN;
  __HAL_SPI_ENABLE(&hspi1);
 
 
 
  HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_RESET);
  HAL_Delay(1);
  HAL_SPI_TransmitReceive(&hspi1,0x9F,0x30,8,0xFF);
  HAL_Delay(1);
  HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET);
 
  while (1)
  {
 
  }
  /* USER CODE END 3 */
}
 
/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
  /** Configure the main internal regulator output voltage 
  */
  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
  /** Initializes the CPU, AHB and APB busses clocks 
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;
  RCC_OscInitStruct.MSIState = RCC_MSI_ON;
  RCC_OscInitStruct.MSICalibrationValue = 0;
  RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_5;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }
  /** Initializes the CPU, AHB and APB busses clocks 
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
  {
    Error_Handler();
  }
}
 
/**
  * @brief SPI1 Initialization Function
  * @param None
  * @retval None
  */
static void MX_SPI1_Init(void)
{
 
  /* USER CODE BEGIN SPI1_Init 0 */
 
  /* USER CODE END SPI1_Init 0 */
 
  /* USER CODE BEGIN SPI1_Init 1 */
 
  /* USER CODE END SPI1_Init 1 */
  /* SPI1 parameter configuration*/
  hspi1.Instance = SPI1;
  hspi1.Init.Mode = SPI_MODE_MASTER;
  hspi1.Init.Direction = SPI_DIRECTION_2LINES;
  hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
  hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
  hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
  hspi1.Init.NSS = SPI_NSS_SOFT;
  hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
  hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
  hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
  hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
  hspi1.Init.CRCPolynomial = 7;
  if (HAL_SPI_Init(&hspi1) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN SPI1_Init 2 */
 
  /* USER CODE END SPI1_Init 2 */
 
}
 
/**
  * @brief GPIO Initialization Function
  * @param None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};
 
  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOA_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();
 
  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_RESET);
 
  /*Configure GPIO pin : PB6 */
  GPIO_InitStruct.Pin = GPIO_PIN_6;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
 
}
 
/* USER CODE BEGIN 4 */
 
/* USER CODE END 4 */
 
/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
 
  /* USER CODE END Error_Handler_Debug */
}
 
#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @param  file: pointer to the source file name
  * @param  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{ 
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

Hello everybody,

i am working with the STM32l011K4T6 and trying to set up the SPI1 to simply transmit a 8-Bit Word to an MRAM Memory.

I have tried a lot of stuff but i cant get the SPI working properly. I included my main.c file which most were automatically created in CubeMX (see pictures of configuration).

Programming and Flashing is done in CubeIDE. For testing i used my Logic Analyzer, and get the screen you see in the picture. "CLK state missmatch idle state". But CPOL and CHPA are both set to 0, in the CLK Register and in the Logic Analyzer.

My Logic-Analyzer pinconfiguration is:

MOSI --> PB5

MISO --> PB4

SCK --> PB3

CS --> PB6

I am using a regular GPIO Output Port (PB6) for Chip Select. Do i have to set/reset some jumpers?

Does anyone have an idea why my clock isnt working?

Thanks for your help!0693W000000WGR2QAO.png0693W000000WGQxQAO.png0693W000000WGQsQAO.png0693W000000WGQnQAO.png

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
TDK
Super User

Initialize the CS pin first and hold it high while you initialize the other pins. Only when you're about to send something should you let it pull it low.

So change

HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_RESET);

to

HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET);

There is a setting in CubeMX to select initial state of the pin.

If you feel a post has answered your question, please click "Accept as Solution".
RSchu.1
Associate II

Hey TDK,

thanks for your reply! I changed the code and in my Logic Analyzer there is no missmatch anymore! But the CLK-Line doesnt look good and on the MOSI Line seemed to be random 8-Bit words. During CS Low there are 8x8 Bits transfered through MOSI in the following order:

0x08 0x00 0x00 0x00 0x00 0x5D 0x1B 0x00

But in my code i just want to send 0x9F and than end the transmission. In CubeMX i could not found any setting for Idle state.0693W000000WH9TQAW.png0693W000000WH9OQAW.png

RSchu.1
Associate II

Second picture is the whole transmission zoomed out. As you can see there is noise on the CLK Line. The first picture is zoomed in into CS LOW transmission. Do you have any ideas?