/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
*****************************************************************...
Second picture is the whole transmission zoomed out. As you can see there is noise on the CLK Line. The first picture is zoomed in into CS LOW transmission. Do you have any ideas?
Hey TDK,thanks for your reply! I changed the code and in my Logic Analyzer there is no missmatch anymore! But the CLK-Line doesnt look good and on the MOSI Line seemed to be random 8-Bit words. During CS Low there are 8x8 Bits transfered through MOSI...