2020-11-12 1:51 AM
Hello,
this is a description of PLL settings from a reference manal
00: The PLL1 input (ref1_ck) clock range frequency is between 1 and 2 MHz (default after reset)
01: The PLL1 input (ref1_ck) clock range frequency is between 2 and 4 MHz
10: The PLL1 input (ref1_ck) clock range frequency is between 4 and 8 MHz
11: The PLL1 input (ref1_ck) clock range frequency is between 8 and 16 MHz
What should I set if my PLL input is exactly at the boundary? Eg 8MHz.
BR
Jan
2020-11-12 3:59 AM
Choose depending on the real frequency 8.000001 or 7.999999 <joke> . Choose any, it should not matter.
2020-11-12 4:14 AM
Thanks for reply. I know that both is working :)
Do you know, what these settings actually do and what happens if the difference would be bigger?
2020-11-12 5:20 PM
PLL is a semi-analog circuit, especially the phase-detector and subsequent filter. There's tradeoff between lock time, jitter and stability in its design. I'd say, this parameter controls this part of the PLL, setting it to a tested optimal state for given input frequency.
> what happens if the difference would be bigger?
Probably the parameters given in DS won't be met under all possible circumstances (power supply voltage range, temperature range).
JW