cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H755xI boot sequence diagram

NGUYEN-VAN NHI
Associate III

Hello guys,

Can anyone help or provide me the boot sequence diagram of STM32H755xI which has dual-core (M7 and M4)?

Thanks a lot !!!

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @NGUYEN-VAN NHI 

Are you looking for this diagram:

Screenshot_2024-08-04-08-13-11-89_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

If not, all available boot diagram you may find on the application note AN2606 or the RM0399.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @NGUYEN-VAN NHI 

Are you looking for this diagram:

Screenshot_2024-08-04-08-13-11-89_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

If not, all available boot diagram you may find on the application note AN2606 or the RM0399.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Dear @STTwo-32 

Thanks for your information. It's beneficial for me.

Regards.

N.V.Nhi