2021-04-28 09:15 AM
Hi all,
I'm editing this post because the forum doesn't allow me to delete it, and it might help someone else..
I was having an issue where simply generating a default NUCLEO-H755ZI-Q project from the current latest CubeMX for Cube IDE and following the debugging instructions in the following application note exactly, did not work.
I tried lots of suggestions on various posts, but for me it turned out to be that the M4 BOOT option byte was disabled, which is why I couldn't debug the M4.
I resolved it with the STLink utility.
Cheers
2021-05-11 08:03 AM
Thank you @Community member for updating your post to share the solution.
This will help other community members finding answers to their issues 😉
Imen