cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H753 - Unused USB connection

Manikandan
Associate II

Hi Team,

 

we are using the STM32H753VI in our design.

we are not using the USB interfaces.

In this case, what is the termination to be done to the VDD33USB pin of STM whether it can be NC, GND?

 

Thanks

Manikandan R

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Manikandan 

My college @FBL has a very good FAQ on that: https://community.st.com/t5/stm32-mcus/faq-configuring-the-vdd50usb-and-vdd33usb-pins-on-stm32h7-when/ta-p/727887.

It should be helpful.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @Manikandan 

My college @FBL has a very good FAQ on that: https://community.st.com/t5/stm32-mcus/faq-configuring-the-vdd50usb-and-vdd33usb-pins-on-stm32h7-when/ta-p/727887.

It should be helpful.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.