2021-08-03 08:02 PM
I had using STM32CubeIDE to generate ADC1 single channel with Timer 6 trigger on 1sec. In HAL library, everything work perfectly and I can see ADC interrupt happen exactly on 1sec interval. But when switch to LL library, same project but the interrupt happen slightly delay, like 1.052s. Just curious what's causing this? can anyone point me out. Thanks
Below is my sample code:
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
LL_APB4_GRP1_EnableClock(LL_APB4_GRP1_PERIPH_SYSCFG);
NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);
/* System interrupt init*/
/* SysTick_IRQn interrupt configuration */
NVIC_SetPriority(SysTick_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),15, 0));
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* Configure the peripherals common clocks */
PeriphCommonClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_ADC1_Init();
MX_TIM6_Init();
/* USER CODE BEGIN 2 */
// HAL_ADCEx_Calibration_Start(&hadc1, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED);
// HAL_TIM_Base_Start(&htim6);
// HAL_ADC_Start_IT(&hadc1);
LL_ADC_SetChannelPreSelection(ADC1, LL_ADC_CHANNEL_3);
LL_ADC_StartCalibration(ADC1, LL_ADC_CALIB_OFFSET, LL_ADC_SINGLE_ENDED);
while( LL_ADC_IsCalibrationOnGoing(ADC1));
LL_TIM_EnableCounter(TIM6);
LL_ADC_REG_SetDataTransferMode(ADC1, LL_ADC_REG_DR_TRANSFER);
LL_ADC_EnableIT_EOC(ADC1);
LL_ADC_Enable(ADC1);
while(LL_ADC_IsActiveFlag_ADRDY(ADC1) != SET);
LL_ADC_REG_StartConversion(ADC1);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
void SystemClock_Config(void)
{
LL_FLASH_SetLatency(LL_FLASH_LATENCY_2);
while(LL_FLASH_GetLatency()!= LL_FLASH_LATENCY_2)
{
}
LL_PWR_ConfigSupply(LL_PWR_LDO_SUPPLY);
LL_PWR_SetRegulVoltageScaling(LL_PWR_REGU_VOLTAGE_SCALE2);
LL_RCC_HSI_Enable();
/* Wait till HSI is ready */
while(LL_RCC_HSI_IsReady() != 1)
{
}
LL_RCC_HSI_SetCalibTrimming(32);
LL_RCC_HSI_SetDivider(LL_RCC_HSI_DIV1);
LL_RCC_PLL_SetSource(LL_RCC_PLLSOURCE_HSI);
LL_RCC_PLL1P_Enable();
LL_RCC_PLL1_SetVCOInputRange(LL_RCC_PLLINPUTRANGE_8_16);
LL_RCC_PLL1_SetVCOOutputRange(LL_RCC_PLLVCORANGE_WIDE);
LL_RCC_PLL1_SetM(4);
LL_RCC_PLL1_SetN(30);
LL_RCC_PLL1_SetP(2);
LL_RCC_PLL1_SetQ(2);
LL_RCC_PLL1_SetR(2);
LL_RCC_PLL1_Enable();
/* Wait till PLL is ready */
while(LL_RCC_PLL1_IsReady() != 1)
{
}
/* Intermediate AHB prescaler 2 when target frequency clock is higher than 80 MHz */
LL_RCC_SetAHBPrescaler(LL_RCC_AHB_DIV_2);
LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_PLL1);
LL_RCC_SetSysPrescaler(LL_RCC_SYSCLK_DIV_1);
LL_RCC_SetAHBPrescaler(LL_RCC_AHB_DIV_2);
LL_RCC_SetAPB1Prescaler(LL_RCC_APB1_DIV_1);
LL_RCC_SetAPB2Prescaler(LL_RCC_APB2_DIV_1);
LL_RCC_SetAPB3Prescaler(LL_RCC_APB3_DIV_1);
LL_RCC_SetAPB4Prescaler(LL_RCC_APB4_DIV_1);
LL_Init1msTick(240000000);
LL_SetSystemCoreClock(240000000);
}
void PeriphCommonClock_Config(void)
{
LL_RCC_PLL2P_Enable();
LL_RCC_PLL2_SetVCOInputRange(LL_RCC_PLLINPUTRANGE_8_16);
LL_RCC_PLL2_SetVCOOutputRange(LL_RCC_PLLVCORANGE_MEDIUM);
LL_RCC_PLL2_SetM(4);
LL_RCC_PLL2_SetN(9);
LL_RCC_PLL2_SetP(4);
LL_RCC_PLL2_SetQ(2);
LL_RCC_PLL2_SetR(2);
LL_RCC_PLL2_SetFRACN(3072);
LL_RCC_PLL2FRACN_Enable();
LL_RCC_PLL2_Enable();
/* Wait till PLL is ready */
while(LL_RCC_PLL2_IsReady() != 1)
{
}
}
static void MX_ADC1_Init(void)
{
/* USER CODE BEGIN ADC1_Init 0 */
/* USER CODE END ADC1_Init 0 */
LL_ADC_InitTypeDef ADC_InitStruct = {0};
LL_ADC_REG_InitTypeDef ADC_REG_InitStruct = {0};
LL_ADC_CommonInitTypeDef ADC_CommonInitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
LL_RCC_SetADCClockSource(LL_RCC_ADC_CLKSOURCE_PLL2P);
/* Peripheral clock enable */
LL_AHB1_GRP1_EnableClock(LL_AHB1_GRP1_PERIPH_ADC12);
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOA);
/**ADC1 GPIO Configuration
PA6 ------> ADC1_INP3
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_6;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* ADC1 interrupt Init */
NVIC_SetPriority(ADC_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(),0, 0));
NVIC_EnableIRQ(ADC_IRQn);
/* USER CODE BEGIN ADC1_Init 1 */
/* USER CODE END ADC1_Init 1 */
/** Common config
*/
ADC_InitStruct.Resolution = LL_ADC_RESOLUTION_16B;
ADC_InitStruct.LowPowerMode = LL_ADC_LP_MODE_NONE;
LL_ADC_Init(ADC1, &ADC_InitStruct);
ADC_REG_InitStruct.TriggerSource = LL_ADC_REG_TRIG_EXT_TIM6_TRGO;
ADC_REG_InitStruct.SequencerLength = LL_ADC_REG_SEQ_SCAN_DISABLE;
ADC_REG_InitStruct.SequencerDiscont = DISABLE;
ADC_REG_InitStruct.ContinuousMode = LL_ADC_REG_CONV_SINGLE;
ADC_REG_InitStruct.Overrun = LL_ADC_REG_OVR_DATA_PRESERVED;
LL_ADC_REG_Init(ADC1, &ADC_REG_InitStruct);
LL_ADC_SetOverSamplingScope(ADC1, LL_ADC_OVS_DISABLE);
ADC_CommonInitStruct.CommonClock = LL_ADC_CLOCK_ASYNC_DIV2;
ADC_CommonInitStruct.Multimode = LL_ADC_MULTI_INDEPENDENT;
LL_ADC_CommonInit(__LL_ADC_COMMON_INSTANCE(ADC1), &ADC_CommonInitStruct);
LL_ADC_REG_SetTriggerEdge(ADC1, LL_ADC_REG_TRIG_EXT_RISING);
/* Disable ADC deep power down (enabled by default after reset state) */
LL_ADC_DisableDeepPowerDown(ADC1);
/* Enable ADC internal voltage regulator */
LL_ADC_EnableInternalRegulator(ADC1);
/* Delay for ADC internal voltage regulator stabilization. */
/* Compute number of CPU cycles to wait for, from delay in us. */
/* Note: Variable divided by 2 to compensate partially */
/* CPU processing cycles (depends on compilation optimization). */
/* Note: If system core clock frequency is below 200kHz, wait time */
/* is only a few CPU processing cycles. */
uint32_t wait_loop_index;
wait_loop_index = ((LL_ADC_DELAY_INTERNAL_REGUL_STAB_US * (SystemCoreClock / (100000 * 2))) / 10);
while(wait_loop_index != 0)
{
wait_loop_index--;
}
/** Configure Regular Channel
*/
LL_ADC_REG_SetSequencerRanks(ADC1, LL_ADC_REG_RANK_1, LL_ADC_CHANNEL_3);
LL_ADC_SetChannelSamplingTime(ADC1, LL_ADC_CHANNEL_3, LL_ADC_SAMPLINGTIME_1CYCLE_5);
LL_ADC_SetChannelSingleDiff(ADC1, LL_ADC_CHANNEL_3, LL_ADC_SINGLE_ENDED);
/* USER CODE BEGIN ADC1_Init 2 */
/* USER CODE END ADC1_Init 2 */
}
static void MX_TIM6_Init(void)
{
/* USER CODE BEGIN TIM6_Init 0 */
/* USER CODE END TIM6_Init 0 */
LL_TIM_InitTypeDef TIM_InitStruct = {0};
/* Peripheral clock enable */
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_TIM6);
/* USER CODE BEGIN TIM6_Init 1 */
/* USER CODE END TIM6_Init 1 */
TIM_InitStruct.Prescaler = 11999;
TIM_InitStruct.CounterMode = LL_TIM_COUNTERMODE_UP;
TIM_InitStruct.Autoreload = 9999;
LL_TIM_Init(TIM6, &TIM_InitStruct);
LL_TIM_DisableARRPreload(TIM6);
LL_TIM_SetTriggerOutput(TIM6, LL_TIM_TRGO_UPDATE);
LL_TIM_DisableMasterSlaveMode(TIM6);
/* USER CODE BEGIN TIM6_Init 2 */
/* USER CODE END TIM6_Init 2 */
}
static void MX_GPIO_Init(void)
{
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOE);
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOA);
/**/
LL_GPIO_ResetOutputPin(LED_GPIO_Port, LED_Pin);
/**/
GPIO_InitStruct.Pin = LED_Pin;
GPIO_InitStruct.Mode = LL_GPIO_MODE_OUTPUT;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
LL_GPIO_Init(LED_GPIO_Port, &GPIO_InitStruct);
}
void ADC_IRQHandler(void)
{
/* USER CODE BEGIN ADC_IRQn 0 */
if(LL_ADC_IsActiveFlag_EOC(ADC1) != RESET)
{
LL_GPIO_TogglePin(LED_GPIO_Port, LED_Pin);
LL_ADC_ClearFlag_EOC(ADC1);
}
/* USER CODE END ADC_IRQn 0 */
/* USER CODE BEGIN ADC_IRQn 1 */
/* USER CODE END ADC_IRQn 1 */
}
Solved! Go to Solution.
2021-08-04 07:23 AM
> LL_RCC_HSI_SetCalibTrimming(32);
Comment out this line and try again.
2021-08-03 10:00 PM
Using HSI as primary clock instead of HSE?
JW
2021-08-03 10:13 PM
For this simple demo example,
I did not enable external clock.
But I don't think this could be the issue.
As same setting, HAL vs LL should give same result.
Unless something is miss on the LL Code.
2021-08-03 10:42 PM
Read our register content of TIM and ADC in both versions and compare.
Set just the timer alone, to see whether difference is in timer's settings or ADC's.
JW
2021-08-04 07:23 AM
> LL_RCC_HSI_SetCalibTrimming(32);
Comment out this line and try again.
2021-08-04 04:47 PM
Thanks and it's work!
Could you explain why this need to comment out?
2021-08-04 05:09 PM
The LL library has a history of setting the wrong HSI calibration value, which makes your clock off by a few %, enough to throw off the UART communication. By commenting it out, you use the default, correct value which is set when the chip comes out of reset.
If you go to the reference manual and look up what the default value is, no doubt it is not 32 but maybe 16 or 64.
Please mark the post that helped you as the best answer if you feel it solved your issue.
2021-08-04 05:49 PM
Thanks for your explanation. I had marked the best answer.
2021-08-04 07:34 PM
Thanks @TDK for point out the problem.
I found out that I had mistakenly set the product revision to Y instead of V.
Set it to V revision solve the issue.