2019-03-08 3:43 AM
About to put my first device in the programmer and don't want to make a mistake. Datasheet says there is a round mark in the corner near pin 1, but of course the package has two round marks on diametrically opposite corners. With the writing correct way up, is it the small circle in bottom left or the larger circle in top right that marks Pin 1 ? I think it's the bottom left as that would match my F407s which don't have this top right circle, but best to make sure first.
2019-03-08 3:46 AM
Look at the datasheet 7 Package information
When you can read the text, Pin 1 is left down.
2019-03-08 3:50 AM
Thanks. Confirms what I thought but the circle in top right is far more prominent and datasheet section 7 doesn't show writing. I got caught once before with an Infineon device having the writing upside down to how I expected so thought it best to check.
Thanks again.