2024-02-19 06:11 AM
Hello everyone,
I am currently working on the SMT32H747i_DISCO board and I was wondering if it is possible to use the Segger J-Link debugger on the Board. There is a j-tag pin out connected to the Dev board which suggests that it should be possible. I didn't have any luck so far. Are there additional ports necessary? Am I missing something. I can't find any documentation to the purpose of the connection. Thanks for any help.
Regards Maikel
2024-02-19 08:43 AM
I'm sorry I made a mistake. I did use the SWO connector for communications. It is however not working with the J-Link adapter.
2024-02-21 04:01 AM
ST also have a page on resolving debugger connection issues:
https://community.st.com/t5/stm32-mcus/how-to-solve-debugger-connection-issues/ta-p/49693