cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743VIT6. FMC for SDRAM

OIrin.1
Associate II

Hi,

Is SDRAM over FMC supported in STM32H743VIT6 MCUs? I can't see this option in CubeMX, only NOR Flash/PSRAM/SRAM/ROM/LCD and NAND Flash. The datasheet says that SDRAM is not supported in LQFP144 packages, but my one is LQFP100.

Looking forward for any help.

4 REPLIES 4

Even fewer pins, so assuming more of the pins you'd need are absent...

Try the Data Sheet and then play Pin Bingo

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

FMC_SDNRAS, FMC_SDNCAS ?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TDK
Guru

SDRAM is not available on the LQFP100 either. FMC_A0, among many others, is absent on the pinout.

If you feel a post has answered your question, please click "Accept as Solution".
OIrin.1
Associate II

Thank you very much Tesla and TDK. I have checked the pinout once more and now I see that some necessary pins for SDRAM support are absent in LQFP100 package. It's a pity.